Other Parts Discussed in Thread: WL1271
Hi,
I am running ICS on pandaboard. For that I am trying to make SD card self bootable but when it starts booting from SD card it is showing kernel panic. The log I am getting is :
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Initializing cgroup subsys cpu
[ 0.000000] Linux version 3.0.1-g000d4b0 (dashwinee@dashwinee) (gcc version 4.4.3 (GCC) ) #1 SMP PREEMPT Fri Feb 24 11:32:46 IST 2012
[ 0.000000] CPU: ARMv7 Processor [411fc092] revision 2 (ARMv7), cr=10c5387f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: OMAP4 Panda board
[ 0.000000] Truncating RAM at 80000000-bfffffff to -afffffff (vmalloc region overlap).
[ 0.000000] Truncating RAM at a0000000-bfffffff to -afffffff (vmalloc region overlap).
[ 0.000000] Reserving 33554432 bytes SDRAM for VRAM
[ 0.000000] Memory policy: ECC disabled, Data cache writealloc
[ 0.000000] OMAP4430 ES2.1
[ 0.000000] SRAM: Mapped pa 0x40300000 to va 0xfe400000 size: 0xd000
[ 0.000000] PERCPU: Embedded 7 pages/cpu @c0e98000 s6912 r8192 d13568 u32768
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 185088
[ 0.000000] Kernel command line: console=ttyO2,115200n8 mem=1G androidboot.console=ttyO2 console=ttyO2,115200n8 androidboot.console=ttyO2 mem=456M@0x80000000 mem=512M@0xA0000000 root=/dev/mmcblk0p2 rw rootdelay=5 init=/init ip=dhcp smsc95xx.macaddr=00:04:9f:00:ea:d3 vram=32M omapfb.vram=0:16M omapdss.def_disp=hdmi consoleblank=0
[ 0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
[ 0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
[ 0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
[ 0.000000] Memory: 729MB = 729MB total
[ 0.000000] Memory: 730704k/1404064k available, 111456k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffc00000 - 0xffe00000 ( 2 MB)
[ 0.000000] vmalloc : 0xf0800000 - 0xf8000000 ( 120 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xf0000000 ( 768 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .init : 0xc0008000 - 0xc0044000 ( 240 kB)
[ 0.000000] .text : 0xc0044000 - 0xc06e4000 (6784 kB)
[ 0.000000] .data : 0xc06e4000 - 0xc0742c80 ( 380 kB)
[ 0.000000] .bss : 0xc0742ca4 - 0xc088d7b8 (1323 kB)
[ 0.000000] SLUB: Genslabs=13, HWalign=32, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
[ 0.000000] Preemptible hierarchical RCU implementation.
[ 0.000000] NR_IRQS:410
[ 0.000000] omap_hwmod: dpll_mpu_m2_ck: missing clockdomain for dpll_mpu_m2_ck.
[ 0.000000] OMAP clockevent source: GPTIMER1 at 32768 Hz
[ 0.000000] sched_clock: 32 bits at 32kHz, resolution 30517ns, wraps every 131071999ms
[ 0.000000] Calibrating delay loop... 2007.19 BogoMIPS (lpj=7839744)
[ 0.015686] pid_max: default: 32768 minimum: 301
[ 0.015686] Mount-cache hash table entries: 512
[ 0.071533] Initializing cgroup subsys debug
[ 0.071563] Initializing cgroup subsys cpuacct
[ 0.071563] Initializing cgroup subsys freezer
[ 0.071624] CPU: Testing write buffer coherency: ok
[ 0.071899] L310 cache controller enabled
[ 0.072021] l2x0: 16 ways, CACHE_ID 0x410000c4, AUX_CTRL 0x5e470000, Cache size: 1048576 B
[ 0.150146] CPU1: Booted secondary processor
[ 0.220458] Brought up 2 CPUs
[ 0.220489] SMP: Total of 2 processors activated (4022.78 BogoMIPS).
[ 0.223144] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for emif_fw
[ 0.223144] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l3_instr
[ 0.223144] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l3_main_1
[ 0.223175] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l3_main_2
[ 0.223175] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_abe
[ 0.223175] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_cfg
[ 0.223205] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_per
[ 0.223205] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for l4_wkup
[ 0.223205] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for mpu_private
[ 0.223266] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for sl2if
[ 0.223266] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for usbhs_ohci
[ 0.223327] omap_hwmod: _populate_mpu_rt_base found no _mpu_rt_va for usbhs_ehci
[ 0.223327] omap_hwmod: l3_div_ck: missing clockdomain for l3_div_ck.
[ 0.231231] omap_hwmod: mcpdm: cannot be enabled (3)
[ 0.233215] print_constraints: dummy:
[ 0.233581] NET: Registered protocol family 16
[ 0.233947] GPMC revision 6.0
[ 0.234832] EMIF0 is enabled with IRQ142
[ 0.234832] EMIF1 is enabled with IRQ143
[ 0.234924] Last reset was cold reset (PRM_RSTST=0x1)
[ 0.234924]
[ 0.234954] HSI: device registered as omap_hwmod: hsi
[ 0.235351] OMAP GPIO hardware version 0.1
[ 0.236236] omap_mux_init: Add partition: #1: core, flags: 2
[ 0.236236] omap_mux_init: Add partition: #2: wkup, flags: 2
[ 0.236236] omap_mux_get_by_name: Could not find signal uart1_cts.uart1_cts
[ 0.238342] omap_hwmod_mux_init: Could not allocate device mux entry
[ 0.247497] OMAP DMA hardware revision 0.0
[ 0.252990] bio: create slab <bio-0> at 0
[ 0.253173] print_constraints: vwl1271: 1800 mV
[ 0.253997] SCSI subsystem initialized
[ 0.254150] usbcore: registered new interface driver usbfs
[ 0.254150] usbcore: registered new interface driver hub
[ 0.254333] usbcore: registered new device driver usb
[ 0.267303] omap_i2c omap_i2c.1: bus 1 rev4.0 at 400 kHz
[ 0.267822] Skipping twl internal clock init and using bootloader value (unknown osc rate)
[ 0.267822] twl6030: PIH (irq 39) chaining IRQs 368..387
[ 0.269714] print_constraints: VUSB: 3300 mV normal standby
[ 0.472717] twl6030_usb twl6030_usb: Initialized TWL6030 USB module
[ 0.473663] print_constraints: VMMC: 1200 <--> 3000 mV at 3000 mV normal standby
[ 0.474151] print_constraints: VPP: 1800 <--> 2500 mV at 1900 mV normal standby
[ 0.474151] print_constraints: VCXIO: 1800 mV normal standby
[ 0.474670] print_constraints: VDAC: 1800 mV normal standby
[ 0.475067] print_constraints: VAUX2_6030: 1200 <--> 2800 mV at 1800 mV normal standby
[ 0.475463] print_constraints: VAUX3_6030: 1000 <--> 3000 mV at 1200 mV normal standby
[ 0.476226] print_constraints: CLK32KG:
[ 0.476226] print_constraints: VANA: 2100 mV normal standby
[ 0.486053] omap_i2c omap_i2c.2: bus 2 rev4.0 at 400 kHz
[ 0.501678] omap_i2c omap_i2c.3: bus 3 rev4.0 at 100 kHz
[ 0.517303] omap_i2c omap_i2c.4: bus 4 rev4.0 at 400 kHz
[ 0.517303] omap-rproc omap-rproc.0: dsp is available
[ 0.517303] omap-rproc omap-rproc.1: ipu is available
[ 0.517944] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.518463] Bluetooth: Core ver 2.16
[ 0.518463] NET: Registered protocol family 31
[ 0.518524] Bluetooth: HCI device and connection manager initialized
[ 0.518524] Bluetooth: HCI socket layer initialized
[ 0.518524] Bluetooth: L2CAP socket layer initialized
[ 0.518524] Bluetooth: SCO socket layer initialized
[ 0.518951] cfg80211: Calling CRDA to update world regulatory domain
[ 0.519012] Switching to clocksource 32k_counter
[ 0.522613] musb-hdrc: version 6.0, musb-dma, peripheral
[ 0.522827] musb-hdrc musb-hdrc: USB Peripheral mode controller at fc0ab000 using DMA, IRQ 124
[ 0.523193] NET: Registered protocol family 2
[ 0.523193] IP route cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.523193] TCP established hash table entries: 131072 (order: 8, 1048576 bytes)
[ 0.525115] Switched to NOHz mode on CPU #0
[ 0.525146] Switched to NOHz mode on CPU #1
[ 0.525177] TCP bind hash table entries: 65536 (order: 8, 1572864 bytes)
[ 0.529846] TCP: Hash tables configured (established 131072 bind 65536)
[ 0.531799] TCP reno registered
[ 0.531799] UDP hash table entries: 512 (order: 3, 32768 bytes)
[ 0.531799] UDP-Lite hash table entries: 512 (order: 3, 32768 bytes)
[ 0.532531] NET: Registered protocol family 1
[ 0.769714] omap-iommu omap-iommu.0: ducati registered
[ 0.769714] omap-iommu omap-iommu.1: tesla registered
[ 0.806549] ashmem: initialized
[ 0.810638] fuse init (API version 7.16)
[ 0.810638] msgmni has been set to 1427
[ 0.813995] io scheduler noop registered
[ 0.813995] io scheduler deadline registered
[ 0.814086] io scheduler cfq registered (default)
[ 0.814086] start plist test
[ 0.818450] end plist test
[ 0.821990] OMAP DSS rev 4.0
[ 0.826568] dsscomp: initializing.
[ 0.826660] misc dsscomp: found 2 displays and 4 overlays
[ 0.826904] could not allocate slot
[ 0.827178] omap-rproc omap-rproc.1: powering up ipu
[ 0.827270] virtio_rpmsg_bus virtio0: rpmsg backend virtproc probed successfully
[ 0.828063] virtio_rpmsg_bus virtio1: rpmsg backend virtproc probed successfully
[ 0.828521] omap_uart.0: ttyO0 at MMIO 0x4806a000 (irq = 104) is a OMAP UART0
[ 0.863525] omap_uart.1: ttyO1 at MMIO 0x4806c000 (irq = 105) is a OMAP UART1
[ 0.905731] omap_uart.2: ttyO2 at MMIO 0x48020000 (irq = 106) is a OMAP UART2
[ 1.801147] console [ttyO2] enabled
[ 1.872894] omap_uart.3: ttyO3 at MMIO 0x4806e000 (irq = 102) is a OMAP UART3
[ 2.021423] PVR: PVRCore_Init
[ 2.024871] PVR: PVRSRVDriverProbe(pDevice=ed4ace00)
[ 2.030517] PVR: SGX register base: 0x56000000
[ 2.035461] PVR: SGX register size: 65535
[ 2.039886] PVR: SGX IRQ: 53
[ 2.043090] PVR: EnableSystemClocks: Enabling System Clocks
[ 2.049255] PVR_K:(Warning): EnableSGXClocks: Unable to scale SGX frequency (EBUSY) [200, drivers/gpu/pvr/omap4/sysutils_linux.c]
[ 2.062194] PVR_K:(Warning): DisableSGXClocks: Unable to scale SGX frequency (EBUSY) [275, drivers/gpu/pvr/omap4/sysutils_linux.c]
[ 2.075256] PVR: PVRCore_Init: major device 251
[ 2.085754] brd: module loaded
[ 2.091949] loop: module loaded
[ 2.097839] PPP generic driver version 2.4.2
[ 2.103088] PPP Deflate Compression module registered
[ 2.103088] PPP BSD Compression module registered
[ 2.114471] PPP MPPE Compression module registered
[ 2.119750] NET: Registered protocol family 24
[ 2.126251] usbcore: registered new interface driver asix
[ 2.132202] usbcore: registered new interface driver cdc_ether
[ 2.138793] usbcore: registered new interface driver smsc95xx
[ 2.145172] usbcore: registered new interface driver net1080
[ 2.151458] usbcore: registered new interface driver cdc_subset
[ 2.158050] usbcore: registered new interface driver zaurus
[ 2.164215] cdc_ncm: 01-June-2011
[ 2.164794] usbcore: registered new interface driver cdc_ncm
[ 2.174224] usbcore: registered new interface driver zd1201
[ 2.180419] ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver
[ 2.187805] ehci-omap ehci-omap.0: OMAP-EHCI Host Controller
[ 2.194122] ehci-omap ehci-omap.0: new USB bus registered, assigned bus number 1
[ 2.202331] ehci-omap ehci-omap.0: irq 109, io mem 0x4a064c00
[ 2.222869] ehci-omap ehci-omap.0: USB 2.0 started, EHCI 1.00
[ 2.229248] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 2.236694] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 2.244628] usb usb1: Product: OMAP-EHCI Host Controller
[ 2.250457] usb usb1: Manufacturer: Linux 3.0.1-g000d4b0 ehci_hcd
[ 2.250518] usb usb1: SerialNumber: ehci-omap.0
[ 2.262542] hub 1-0:1.0: USB hub found
[ 2.266662] hub 1-0:1.0: 3 ports detected
[ 2.304992] usbcore: registered new interface driver cdc_acm
[ 2.311340] cdc_acm: USB Abstract Control Model driver for USB modems and ISDN adapters
[ 2.320098] Initializing USB Mass Storage driver...
[ 2.325592] usbcore: registered new interface driver usb-storage
[ 2.332153] USB Mass Storage support registered.
[ 2.337371] usbcore: registered new interface driver usbserial
[ 2.343750] usbserial: USB Serial Driver core
[ 2.348602] USB Serial support registered for Keyspan - (without firmware)
[ 2.356170] USB Serial support registered for Keyspan 1 port adapter
[ 2.363159] USB Serial support registered for Keyspan 2 port adapter
[ 2.370178] USB Serial support registered for Keyspan 4 port adapter
[ 2.377227] usbcore: registered new interface driver keyspan
[ 2.383483] keyspan: v1.1.5:Keyspan USB to Serial Converter Driver
[ 2.592102] android_usb gadget: Mass Storage Function, version: 2009/09/11
[ 2.599639] android_usb gadget: Number of LUNs=1
[ 2.604705] lun0: LUN: removable file: (no medium)
[ 2.610168] android_usb gadget: android_usb ready
[ 2.615539] mousedev: PS/2 mouse device common for all mice
[ 2.621917] i2c /dev entries driver
[ 2.626770] lirc_dev: IR Remote Control driver registered, major 249
[ 2.633666] usb 1-1: new high speed USB device number 2 using ehci-omap
[ 2.640991] IR NEC protocol handler initialized
[ 2.645904] IR RC5(x) protocol handler initialized
[ 2.651092] IR RC6 protocol handler initialized
[ 2.655975] IR JVC protocol handler initialized
[ 2.660919] IR Sony protocol handler initialized
[ 2.665924] IR RC5 (streamzap) protocol handler initialized
[ 2.671997] IR LIRC bridge handler initialized
[ 2.676879] dmm: probe base: fd300000, irq 145
[ 2.683715] device-mapper: uevent: version 1.0.3
[ 2.688812] device-mapper: ioctl: 4.20.0-ioctl (2011-02-02) initialised: dm-devel@redhat.com
[ 2.698211] Bluetooth: HCI UART driver ver 2.2
[ 2.703033] Bluetooth: HCI H4 protocol initialized
[ 2.708251] cpuidle: using governor ladder
[ 2.712738] cpuidle: using governor menu
[ 2.721832] usbcore: registered new interface driver usbhid
[ 2.727935] usbhid: USB HID core driver
[ 2.732269] logger: created 256K log 'log_main'
[ 2.737548] logger: created 256K log 'log_events'
[ 2.742950] logger: created 256K log 'log_radio'
[ 2.748077] logger: created 256K log 'log_system'
[ 2.754089] OMAP HSI: HSI DRIVER Version 0.4.1
[ 2.759033] omap_hsi omap_hsi.0: Registering IRQ mpu_p1 (99)
[ 2.765380] omap_hsi omap_hsi.0: Registering IRQ mpu_dma (103)
[ 2.771911] omap_hsi omap_hsi.0: HSI Hardware REVISION 0x50043101
[ 2.787750] SDP4430 SoC init
[ 2.810028] usb 1-1: New USB device found, idVendor=0424, idProduct=9514
[ 2.817352] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 2.825683] hub 1-1:1.0: USB hub found
[ 2.829895] hub 1-1:1.0: 5 ports detected
[ 2.838409] asoc: null-codec-dai <-> MultiMedia1 mapping ok
[ 2.844879] asoc: null-codec-dai <-> MultiMedia2 mapping ok
[ 2.851806] asoc: null-codec-dai <-> Voice mapping ok
[ 2.858825] asoc: null-codec-dai <-> Tones mapping ok
[ 2.865173] asoc: null-codec-dai <-> Vibra mapping ok
[ 2.871307] asoc: null-codec-dai <-> MODEM mapping ok
[ 2.877227] asoc: null-codec-dai <-> MultiMedia1 LP mapping ok
[ 2.884124] asoc: FM Digital <-> omap-mcbsp-dai.1 mapping ok
[ 2.891723] asoc: twl6040-dl1 <-> mcpdm-dl mapping ok
[ 2.898498] twl6040-codec twl6040-codec: ASoC: Failed to create Aux/FM Stereo In debugfs file
[ 2.908538] asoc: twl6040-dl1 <-> mcpdm-dl1 mapping ok
[ 2.914855] asoc: twl6040-ul <-> mcpdm-ul1 mapping ok
[ 2.920928] asoc: twl6040-dl2 <-> mcpdm-dl2 mapping ok
[ 2.927276] asoc: twl6040-vib <-> mcpdm-vib mapping ok
[ 2.933441] asoc: Bluetooth <-> omap-mcbsp-dai.0 mapping ok
[ 2.940643] asoc: Bluetooth <-> omap-mcbsp-dai.0 mapping ok
[ 2.946777] mmc0: host does not support reading read-only switch. assuming write-enable.
[ 2.956146] asoc: FM Digital <-> omap-mcbsp-dai.1 mapping ok
[ 2.962799] asoc: MODEM <-> omap-mcbsp-dai.1 mapping ok
[ 2.968688] mmc0: new SDHC card at address e624
[ 2.973999] input: Panda Headset Jack as /devices/platform/soc-audio/sound/card0/input0
[ 2.984008] mmcblk0: mmc0:e624 SD04G 3.69 GiB
[ 2.990783] ALSA device list:
[ 2.993988] #0: TI OMAP4 Board
[ 2.997589] mmcblk0: p1 p2
[ 3.004180] GACT probability NOT on
[ 3.007995] Mirror/redirect action on
[ 3.019714] u32 classifier
[ 3.022644] Actions configured
[ 3.026367] Netfilter messages via NETLINK v0.30.
[ 3.043853] nf_conntrack version 0.5.0 (11417 buckets, 45668 max)
[ 3.059661] ctnetlink v0.93: registering with nfnetlink.
[ 3.065734] xt_time: kernel timezone is -0000
[ 3.083923] ip_tables: (C) 2000-2006 Netfilter Core Team
[ 3.089813] arp_tables: (C) 2002 David S. Miller
[ 3.097930] TCP cubic registered
[ 3.102111] NET: Registered protocol family 10
[ 3.111389] Mobile IPv6
[ 3.114074] IPv6 over IPv4 tunneling driver
[ 3.122924] NET: Registered protocol family 17
[ 3.127746] NET: Registered protocol family 15
[ 3.129302] usb 1-1.1: new high speed USB device number 3 using ehci-omap
[ 3.139923] Bluetooth: RFCOMM TTY layer initialized
[ 3.145233] Bluetooth: RFCOMM socket layer initialized
[ 3.150756] Bluetooth: RFCOMM ver 1.11
[ 3.154846] NET: Registered protocol family 35
[ 3.160003] lib80211: common routines for IEEE802.11 drivers
[ 3.166168] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 1
[ 3.172698] mmc1: card claims to support voltages below the defined range. These will be ignored.
[ 3.184143] ThumbEE CPU extension supported.
[ 3.188812] Registering SWP/SWPB emulation handler
[ 3.192535] mmc1: queuing unknown CIS tuple 0x91 (3 bytes)
[ 3.193420] mmc1: new SDIO card at address 0001
[ 3.207855] Reprogramming LPDDR2 timings to 400000000 Hz
[ 3.215209] Power Management for TI OMAP4.
[ 3.219848] OMAP4 PM: Static dependency added between MPUSS <-> EMIF, MPUSS <-> L4_PER/CFG MPUSS <-> L3_MAIN_1.
[ 3.230712] OMAP4 PM: Static dependency added between DUCATI <-> L4_PER/CFG and DUCATI <-> L3.
[ 3.247680] clock: disabling unused clocks to save power
[ 3.258728] usb 1-1.1: New USB device found, idVendor=0424, idProduct=ec00
[ 3.259643] cannot apply mgr(lcd) on inactive device
[ 3.259765] omapfb omapfb: failed to apply dispc config
[ 3.262725] cannot apply mgr(tv) on inactive device
[ 3.262847] omapfb omapfb: failed to apply dispc config
[ 3.265838] cannot apply mgr(lcd2) on inactive device
[ 3.265930] omapfb omapfb: failed to apply dispc config
[ 3.265930] omapfb omapfb: cannot find default display
[ 3.304382] usb 1-1.1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[ 3.312408] regulator_init_complete: VANA: incomplete constraints, leaving on
[ 3.314758] smsc95xx v1.0.4
[ 3.324707] regulator_init_complete: VDAC: incomplete constraints, leaving on
[ 3.332672] regulator_init_complete: VCXIO: incomplete constraints, leaving on
[ 3.341125] omaplfb: OMAPLFB_Init: OMAPLFBInit failed
[ 3.346740] drivers/rtc/hctosys.c: unable to open rtc device (rtc0)
[ 3.354156] Waiting 5sec before mounting root device...
[ 3.402923] smsc95xx 1-1.1:1.0: eth0: register 'smsc95xx' at usb-ehci-omap.0-1.1, smsc95xx USB 2.0 Ethernet, 06:8e:5d:0a:9a:4f
[ 3.500518] usb 1-1.2: new low speed USB device number 4 using ehci-omap
[ 3.632019] usb 1-1.2: New USB device found, idVendor=413c, idProduct=2003
[ 3.639465] usb 1-1.2: New USB device strings: Mfr=1, Product=2, SerialNumber=0
[ 3.647338] usb 1-1.2: Product: Dell USB Keyboard
[ 3.652435] usb 1-1.2: Manufacturer: Dell
[ 3.661682] input: Dell Dell USB Keyboard as /devices/platform/omap/usbhs_omap/ehci-omap.0/usb1/1-1/1-1.2/1-1.2:1.0/input/input1
[ 3.675201] generic-usb 0003:413C:2003.0001: input: USB HID v1.10 Keyboard [Dell Dell USB Keyboard] on usb-ehci-omap.0-1.2/input0
[ 3.770843] usb 1-1.3: new low speed USB device number 5 using ehci-omap
[ 3.902557] usb 1-1.3: New USB device found, idVendor=0461, idProduct=4d15
[ 3.909912] usb 1-1.3: New USB device strings: Mfr=0, Product=2, SerialNumber=0
[ 3.917724] usb 1-1.3: Product: USB Optical Mouse
[ 3.926055] input: USB Optical Mouse as /devices/platform/omap/usbhs_omap/ehci-omap.0/usb1/1-1/1-1.3/1-1.3:1.0/input/input2
[ 3.938476] generic-usb 0003:0461:4D15.0002: input: USB HID v1.11 Mouse [USB Optical Mouse] on usb-ehci-omap.0-1.3/input0
[ 61.004150] omap-rproc omap-rproc.1: rproc_loader_cont: failed to load ducati-m3.bin
[ 64.192535] wl1271: ERROR could not get nvs file: -2
[ 64.203186] wl1271: loaded
[ 64.203186] wl1271: initialized
[ 64.216857] EXT2-fs (mmcblk0p2): error: couldn't mount because of unsupported optional features (240)
[ 64.287261] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities
[ 64.418426] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
[ 64.428161] VFS: Mounted root (ext4 filesystem) on device 179:2.
[ 64.434875] Freeing init memory: 240K
[ 64.474731] init (1): /proc/1/oom_adj is deprecated, please use /proc/1/oom_score_adj instead.
[ 79.040496] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
[ 79.280639] init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
[ 79.294738] android_usb: already disabled
[ 79.300170] adb_bind_config
[ 79.531616] PVR: Installing MISR with cookie c0783adc
[ 79.537445] PVR: Installing device LISR SGX ISR on IRQ 53 with cookie ed4a4500
[ 79.546081] PVR: OSUnMapPhysToLin: unmapping 65535 bytes from f0b20000
[ 79.553985] PVR: SysFinalise: Version string: SGX revision = 1.2.0
shell@android:/ $ [ 79.715606] adb_open
[ 79.940887] adb_release
[ 79.944030] adb_open
[ 79.946899] adb_bind_config
[ 80.666778] init: untracked pid 84 exited
[ 80.672088] Kernel panic - not syncing: Attempted to kill init!
[ 80.678619] Backtrace:
[ 80.681457] [<c004e980>] (dump_backtrace+0x0/0x10c) from [<c052ca70>] (dump_stack+0x18/0x1c)
[ 80.690643] r7:ed43c000 r6:ed440000 r5:c0717d8c r4:c0745968
[ 80.695373] [<c052ca58>] (dump_stack+0x0/0x1c) from [<c052caf0>] (panic+0x7c/0x1c0)
[ 80.705535] [<c052ca74>] (panic+0x0/0x1c0) from [<c008febc>] (do_exit+0x634/0x6e0)
[ 80.713867] r3:c0717d8c r2:00000000 r1:ed43c000 r0:c065ed2c
[ 80.720153] [<c008f888>] (do_exit+0x0/0x6e0) from [<c008ffac>] (do_group_exit+0x44/0xc4)
[ 80.728912] [<c008ff68>] (do_group_exit+0x0/0xc4) from [<c009c918>] (get_signal_to_deliver+0x1f4/0x430)
[ 80.739135] r7:ed442000 r6:ed441ec8 r5:ed440000 r4:0000000b
[ 80.742248] [<c009c724>] (get_signal_to_deliver+0x0/0x430) from [<c004d7d8>] (do_signal+0x98/0x570)
[ 80.755187] [<c004d740>] (do_signal+0x0/0x570) from [<c004dcf0>] (do_notify_resume+0x40/0x4c)
[ 80.764434] [<c004dcb0>] (do_notify_resume+0x0/0x4c) from [<c004aa58>] (work_pending+0x24/0x28)
[ 80.773956] r5:00000054 r4:ffffffff
[ 80.777648] CPU0: stopping
[ 80.777893] Backtrace:
[ 80.783416] [<c004e980>] (dump_backtrace+0x0/0x10c) from [<c052ca70>] (dump_stack+0x18/0x1c)
[ 80.792449] r7:00000000 r6:c0042e80 r5:c06f6568 r4:ec93a000
[ 80.798553] [<c052ca58>] (dump_stack+0x0/0x1c) from [<c00443b0>] (do_IPI+0x160/0x194)
[ 80.806915] [<c0044250>] (do_IPI+0x0/0x194) from [<c004a728>] (__irq_usr+0x48/0xe0)
[ 80.815093] Exception stack(0xec93bfb0 to 0xec93bff8)
[ 80.820495] bfa0: 404b8cd0 4092e624 03000003 545a5f00
[ 80.829223] bfc0: 01010101 00000035 404b0590 404b0240 404b8700 4092e60e 4092e60e 4098c938
[ 80.837982] bfe0: 4e5a5f00 beb555bc b0003a17 b000145c 40000010 ffffffff
[ 80.845062] Rebooting in 5 seconds..
Somebody please tell me why I am getting this Kernel panic and what is the solution for that?
Thanks in advance.
Regards,
Ashwinee