Part Number: AM3358
Our customer want to use DDR3L (MT41K512M16VRP-107 IT:P) with AM3358BZCZA.
According to the datasheet, for DDR3 and DDR3L, the Zo (single-ended impedance) range is specified as 50 ohm (TYP) to 75 ohm (MAX).
They have found that achieving 50 ohm (TYP) is difficult for their PCB design.
For the Zo (single-ended impedance), is any value within the range of 50 ohm (TYP) to 75 ohm (MAX) acceptable?
If so, is impedance control required within ±5 ohm of the selected target impedance value (Zo)?
Other than 50 ohm (TYP), what value would you recommend?
If a value other than 50 ohm (TYP) is used, are there any precautions or considerations that should be taken into account?
Best regards,
Daisuke