===here is my environment===
Board: TI EVM6437 development board
Emulator: Wintech XDS560V2 trace
Software: CCS5.1.0.09000
package: bios_6_32_05_54
package: C:\dvsdk_1_01_00_15\psp_1_00_02_00
YES,I know BIOSPSP drvier with sys/bios6 does not support for DM6437.
here is my issue:
there are any plans to release BIOSPSP drvier with sys/bios6 support for DM6437??
OR
Can I change BIOSPSP OS folder source file,make it be same with sys/bios6 API??
I want to run a sys/bios6 project with VPFE driver in dm6437.
Anyone can help me?
THANKS,
Yang Hai.