This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

I plus the xio2001 EVM into the dm816x EVM and plus the ethnet pci card intto the xio2001.Why I can not find ethnet pci card?

Other Parts Discussed in Thread: XIO2001

1. When I plus the xio2001 EVM into the dm816x EVM and I use "lspci -v"(do not plus the ethnet pci card intto the xio2001) , the message:

00:00.0 Class 0604: Device 104c:8888 (rev 01)
        Flags: bus master, fast devsel, latency 0
        Memory at <ignored> (32-bit, non-prefetchable)
        Memory at <ignored> (32-bit, prefetchable)
        Bus: primary=00, secondary=01, subordinate=02, sec-latency=0
        Capabilities: [40] Power Management version 3
        Capabilities: [50] MSI: Enable- Count=1/1 Maskable- 64bit+
        Capabilities: [70] Express Root Port (Slot-), MSI 00
        Capabilities: [100] Advanced Error Reporting

01:00.0 Class 0604: Device 104c:8240
        Flags: bus master, fast devsel, latency 0
        Bus: primary=01, secondary=02, subordinate=02, sec-latency=0
        Capabilities: [40] Subsystem: Device 0000:0000
        Capabilities: [48] Power Management version 3
        Capabilities: [50] MSI: Enable- Count=1/16 Maskable- 64bit+
        Capabilities: [70] Express PCI/PCI-X Bridge, MSI 00
        Capabilities: [100] Advanced Error Reporting

2. When I plus the xio2001 EVM into the dm816x EVM and plus the ethnet pci card intto the xio2001,the message is same, I can not find  the ethnet pci card . Why?

3.  When I plus the xio2001 EVM into the PC and plus the ethnet pci card intto the xio2001, I can find the ethnet pci card .