This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Where can I start integration H.264 encoder ?

Hi, all

 

I'm starting H.264 encoder integration for our camera which is using DM6446.

Image size is 320*240 and frame rate is 30Hz. It doesn't have audio circuit.

It is transfering 8 bit raw video data ox 320*240 to PC application program by Ethernet.

Working platform is linux. Base platform had started from dsplink's readwrite samples.

DSP is enhancing image quality and some noise.

 

Now, I've got dm6446_h264enc_2_00_01_00_production.bin and have read H264_Encoder_DM6446_UserGuide.pdf.

But it assumes window platform CCS.

 

Where can I get integration document for Linux platform ?

 

 

Best regads,

G.S.Lee