Other Parts Discussed in Thread: OMAP3530
hi all
i am working OMAP3530,
i have to interface two LPDDR SDRAM's to SDRC.
there are two Chip selects in SDRC, each can support 512 MB, so the
total supported memory is 1GB.
my questions is..
1) what type LPDDR SDRAM Addressing supported can be used, for
example ,LF(JEDEC-standard addressing), L2 (2-die stack standard
addressing), L4 (4-die stack standard addressing), LG(Reduced Page
Size) or R4 (R4 = 4-die stack reduced page-size addressing) ?
thanks and regards
N Reddy