Hi ,
I am running my Android froyo on AM1808 evm. Almost I have followed all the steps based on the forums. We got android froyo prebuilt images from the TI link. We are able to build the images and created the file system.
Finally we are able to mount the filesystem through SD-Card and NFS. Once it is going in to file system there is ANDROID message on the TFT LCD screen. But there is no image after that.
After some time it goes to kernel panic. Please find the below logs for your reference
Looking up port of RPC 100005/1 on 192.168.1.200
VFS: Mounted root (nfs filesystem) on device 0:13.
Freeing init memory: 140K
Warning: unable to open an initial console.
init: cannot open '/initlogo.rle'
init: cannot find '/system/etc/install-recovery.sh', disabling 'flash_recovery'
# warning: `zygote' uses 32-bit capabilities (legacy support in use)
request_suspend_state: wakeup (3->0) at 61283295585 (2012-02-22 15:30:49.752085499 UTC)
init: untracked pid 783 exited
#
#
# ls -l
drwxrwxrwx root root 2012-02-29 05:52 system
dr-x------ root root 2012-02-29 06:01 config
dr-xr-xr-x root root 1970-01-01 00:00 proc
lrwxrwxrwx root root 2012-02-29 06:01 etc -> /system/etc
drwxr-xr-x root root 2012-02-29 06:01 acct
lrwxrwxrwx root root 2012-02-29 06:01 d -> /sys/kernel/debug
drwxr-xr-x root root 2012-02-22 15:30 dev
-rwxrwxrwx root shell 107412 2012-02-29 05:44 init
-rwxrwxrwx root shell 1677 2012-02-29 05:44 init.goldfish.rc
drwxrwx--x system system 2012-02-29 06:01 data
drwxrwxrwx root shell 2012-02-29 05:52 sbin
-rwxrwxrwx root shell 13696 2012-02-29 05:44 init.rc
drwxr-xr-x root root 1970-01-01 00:00 sys
drwxrwxr-x root system 2012-02-29 06:01 mnt
-rwxrwxrwx root root 118 2012-02-29 05:44 default.prop
lrwxrwxrwx root root 2012-02-29 06:01 sdcard -> /mnt/sdcard
drwxrwx--- system cache 2012-02-29 06:01 cache
#
# warning: `zygote' uses 32-bit capabilities (legacy support in use)
request_suspend_state: wakeup (3->0) at 81522464127 (2012-02-22 15:31:09.991176583 UTC)
init: untracked pid 778 exited
Regards,
Francis Kumar