This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can the resizer be used withput the previewer in continuous mode on dm365?

Hello,

I'm a little bit confused by using resizer on dm365 with linux 2.6.32.17 (dvsdk 4.02). Can it be used without the previewer in continuous mode? I need it just to convert UYVY to NV12 for h264 codec. When the previewer is not configured vpfe_dev->imp_chained is not set and resizer is not enabled when calling STREAM_ON ioctl...

best regards
Jan 

  • Jan Pohanka said:

    Hello,

    I'm a little bit confused by using resizer on dm365 with linux 2.6.32.17 (dvsdk 4.02). Can it be used without the previewer in continuous mode? I need it just to convert UYVY to NV12 for h264 codec. When the previewer is not configured vpfe_dev->imp_chained is not set and resizer is not enabled when calling STREAM_ON ioctl...

    best regards
    Jan 

    Of course you can. IPIPE continuous mode like below:

    ISIF-》previerwe-》resizer-》SDRAM

    ISIF-》previewer-》sdram

    ISIF-》resizer-》sdram