This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

NDK2 examples emacHooks.c question.

Hello,

I'm working with C6748, NDK 2.20.05.33, BIOS 5.41.11.38, nsp_1_00_00_09.

In the NSP examples they use emacHooks.c where some EMAC initialization routines written and called from the NDK stack.

  • Do I have to use all these functions to initialize the EMAC driver?
  • Is there a way to prevent using them, and configure the NDK to use its internal HAL ?
Anatoly.