This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Kernel default config file for Gingerbread



The currently distributed default Android kernel config file is out of sync with menuconfig or xconfig.  After setting the default, running xconfig/menuconfig shows the wrong processor and other settings that are in the default.  Also, if you make a change or just save the config in either environment, a subsequent make will force you into the tect only config sequence.  This was not a problem in the Froyo release as I used this quite a bit to port my kernel for my custom board.