This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Codec Engine example error on OMAP3730 EVM/WinCE6



Hello,

I've got the following error mesages:

 213380 PID:400002 TID:2e5002e Configuration error (B): Exceeded maximum number [31] of Translation  Look-aside Buffers.
 213381 PID:400002 TID:2e5002e The configured entries are:
    Number of entries of size 4KB:  1
    Number of buffers of size 64KB: 0
    Number of buffers of size 1MB:  29
    Number of buffers of size 16MB: 2
 213381 PID:400002 TID:2e5002e  DSP_init status [0x80008052]
 213384 PID:22c0072 TID:2e5002e @214,162,000us: [+7 T:0x02e5002e S:0x000afe04] OP - Processor_create_d> Loading and starting DSP server 'Windows\all.x64P' FAILED, status=[0x80008052] (look for error code 'DSP_EBASE + 0x52' in dsplin
 213384 PID:22c0072 TID:2e5002e k*/packages/dsplink/gpp/inc/usr/errbase.h)

when running the audio_copy example with app_remote_wince.exe. I've looked at http://e2e.ti.com/support/dsp/omap_applications_processors/f/42/t/29951.aspx, http://processors.wiki.ti.com/index.php/Codec_Engine_Examples_Memory_Maphttp://processors.wiki.ti.com/index.php/Changing_the_DVEVM_memory_map, and tried to modify the memory configuration. A log with CE_DEBUG=3 and a few configuration files are attached in the zip file.

Another question I have is: should I use all.x64P in ti\sdo\ce\examples\servers\all_codecs_new_config\bin\ti_platforms_evm3530\ or audio_copy.x64P in ti\sdo\ce\examples\servers\server_api_example\bin\ti_platforms_evm3530 instead of the default all.x64P in ti\sdo\ce\examples\servers\all_codecs\bin\ti_platforms_evm3530?

Please help. Thanks,

Ying

all_evm3530.zip