Hello,
I seem to have run into a kernel panic trying to boot the EVM with the 5.03.03 package. This is the default configuration with the stock EVM board. Any help would be appreciated.
U-Boot SPL 2011.09 (Feb 28 2012 - 16:33:00)
Texas Instruments Revision detection unimplemented
U-Boot 2011.09 (Feb 28 2012 - 16:33:00)
I2C: ready
DRAM: 256 MiB
WARNING: Caches not enabled
Found a daughter card connected
NAND: HW ECC Hamming Code selected
256 MiB
MMC: OMAP SD/MMC: 0
Net: cpsw
Hit any key to stop autoboot: 0
link up on port 0, speed 100, full duplex
BOOTP broadcast 1
DHCP client bound to address 192.168.0.58
link up on port 0, speed 100, full duplex
Using cpsw device
TFTP from server 192.168.0.1; our IP address is 192.168.0.58
Filename 'uImage-am335x-evm-htfoo.bin'.
Load address: 0x82000000
Loading: #################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
#################################################################
###################################################
done
Bytes transferred = 2922136 (2c9698 hex)
## Booting kernel from Legacy Image at 82000000 ...
Image Name: Linux-3.1.0
Image Type: ARM Linux Kernel Image (uncompressed)
Data Size: 2922072 Bytes = 2.8 MiB
Load Address: 80008000
Entry Point: 80008000
Verifying Checksum ... OK
Loading Kernel Image ... OK
OK
Starting kernel ...
Uncompressing Linux... done, booting the kernel.
[ 0.000000] Linux version 3.1.0 (htfoo@htfoo-Vostro-3550) (gcc version 4.5.3 20110311 (prerelease) (GCC) ) #1 Wed Feb 29 18:07:00 MYT 2012
[ 0.000000] CPU: ARMv7 Processor [413fc082] revision 2 (ARMv7), cr=10c53c7f
[ 0.000000] CPU: VIPT nonaliasing data cache, VIPT aliasing instruction cache
[ 0.000000] Machine: am335xevm
[ 0.000000] Memory policy: ECC disabled, Data cache writeback
[ 0.000000] AM335X ES1.0 (neon )
[ 0.000000] Built 1 zonelists in Zone order, mobility grouping on. Total pages: 65024
[ 0.000000] Kernel command line: console=ttyO0,115200n8 root=/dev/nfs nfsroot=192.168.0.1:/home/htfoo/firmware/ti-sdk-5.03.02/targetNFS,nolock rw ip=dhcp
[ 0.000000] PID hash table entries: 1024 (order: 0, 4096 bytes)
[ 0.000000] Dentry cache hash table entries: 32768 (order: 5, 131072 bytes)
[ 0.000000] Inode-cache hash table entries: 16384 (order: 4, 65536 bytes)
[ 0.000000] Memory: 256MB = 256MB total
[ 0.000000] Memory: 253724k/253724k available, 8420k reserved, 0K highmem
[ 0.000000] Virtual kernel memory layout:
[ 0.000000] vector : 0xffff0000 - 0xffff1000 ( 4 kB)
[ 0.000000] fixmap : 0xfff00000 - 0xfffe0000 ( 896 kB)
[ 0.000000] DMA : 0xffa00000 - 0xffe00000 ( 4 MB)
[ 0.000000] vmalloc : 0xd0800000 - 0xf8000000 ( 632 MB)
[ 0.000000] lowmem : 0xc0000000 - 0xd0000000 ( 256 MB)
[ 0.000000] modules : 0xbf000000 - 0xc0000000 ( 16 MB)
[ 0.000000] .text : 0xc0008000 - 0xc0534000 (5296 kB)
[ 0.000000] .init : 0xc0534000 - 0xc056d000 ( 228 kB)
[ 0.000000] .data : 0xc056e000 - 0xc05c2d80 ( 340 kB)
[ 0.000000] .bss : 0xc05c2da4 - 0xc05fd320 ( 234 kB)
[ 0.000000] NR_IRQS:396
[ 0.000000] IRQ: Found an INTC at 0xfa200000 (revision 5.0) with 128 interrupts
[ 0.000000] Total of 128 interrupts on 1 active controller
[ 0.000000] OMAP clockevent source: GPTIMER1 at 24000000 Hz
[ 0.000000] OMAP clocksource: GPTIMER2 at 24000000 Hz
[ 0.000000] sched_clock: 32 bits at 24MHz, resolution 41ns, wraps every 178956ms
[ 0.000000] Console: colour dummy device 80x30
[ 0.000199] Calibrating delay loop... 718.02 BogoMIPS (lpj=3590144)
[ 0.059022] pid_max: default: 32768 minimum: 301
[ 0.059146] Security Framework initialized
[ 0.059250] Mount-cache hash table entries: 512
[ 0.059624] CPU: Testing write buffer coherency: ok
[ 0.064156] print_constraints: dummy:
[ 0.064533] NET: Registered protocol family 16
[ 0.064870] GPMC revision 6.0
[ 0.066887] OMAP GPIO hardware version 0.1
[ 0.069033] omap_l3_smx omap_l3_smx.0: couldn't find resource
[ 0.069791] omap_mux_init: Add partition: #1: core, flags: 0
[ 0.072752] omap_i2c.1: alias fck already exists
[ 0.074220] omap2_mcspi.1: alias fck already exists
[ 0.074438] omap2_mcspi.2: alias fck already exists
[ 0.096850] bio: create slab <bio-0> at 0
[ 0.098592] SCSI subsystem initialized
[ 0.101037] usbcore: registered new interface driver usbfs
[ 0.101378] usbcore: registered new interface driver hub
[ 0.101584] usbcore: registered new device driver usb
[ 0.119145] omap_i2c omap_i2c.1: bus 1 rev4.0 at 100 kHz
[ 0.121141] Advanced Linux Sound Architecture Driver Version 1.0.24.
[ 0.122191] Switching to clocksource gp timer
[ 0.129104] Switched to NOHz mode on CPU #0
[ 0.137553] musb-hdrc: version 6.0, ?dma?, otg (peripheral+host)
[ 0.137748] musb-hdrc musb-hdrc.0: dma type: pio
[ 0.138588] musb-hdrc musb-hdrc.0: USB OTG mode controller at d080a000 using PIO, IRQ 18
[ 0.138765] musb-hdrc musb-hdrc.1: dma type: pio
[ 0.139456] musb-hdrc musb-hdrc.1: USB OTG mode controller at d080c800 using PIO, IRQ 19
[ 0.139854] NET: Registered protocol family 2
[ 0.140053] IP route cache hash table entries: 2048 (order: 1, 8192 bytes)
[ 0.140343] TCP established hash table entries: 8192 (order: 4, 65536 bytes)
[ 0.140504] TCP bind hash table entries: 8192 (order: 3, 32768 bytes)
[ 0.140599] TCP: Hash tables configured (established 8192 bind 8192)
[ 0.140611] TCP reno registered
[ 0.140624] UDP hash table entries: 256 (order: 0, 4096 bytes)
[ 0.140647] UDP-Lite hash table entries: 256 (order: 0, 4096 bytes)
[ 0.140831] NET: Registered protocol family 1
[ 0.141114] RPC: Registered named UNIX socket transport module.
[ 0.141129] RPC: Registered udp transport module.
[ 0.141139] RPC: Registered tcp transport module.
[ 0.141148] RPC: Registered tcp NFSv4.1 backchannel transport module.
[ 0.141367] NetWinder Floating Point Emulator V0.97 (double precision)
[ 0.154359] VFS: Disk quotas dquot_6.5.2
[ 0.154429] Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[ 0.154960] JFFS2 version 2.2. (NAND) (SUMMARY) © 2001-2006 Red Hat, Inc.
[ 0.155235] msgmni has been set to 495
[ 0.155993] io scheduler noop registered
[ 0.156007] io scheduler deadline registered
[ 0.156081] io scheduler cfq registered (default)
[ 0.159471] Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled
[ 0.161169] omap_uart.0: ttyO0 at MMIO 0x44e09000 (irq = 72) is a OMAP UART0
[ 0.636404] console [ttyO0] enabled
[ 0.640599] omap_uart.1: ttyO1 at MMIO 0x48022000 (irq = 73) is a OMAP UART1
[ 0.648367] omap_uart.2: ttyO2 at MMIO 0x48024000 (irq = 74) is a OMAP UART2
[ 0.656060] omap_uart.3: ttyO3 at MMIO 0x481a6000 (irq = 44) is a OMAP UART3
[ 0.663739] omap_uart.4: ttyO4 at MMIO 0x481a8000 (irq = 45) is a OMAP UART4
[ 0.671375] omap_uart.5: ttyO5 at MMIO 0x481aa000 (irq = 46) is a OMAP UART5
[ 0.687559] brd: module loaded
[ 0.695677] loop: module loaded
[ 0.699126] i2c-core: driver [tsl2550] using legacy suspend method
[ 0.705615] i2c-core: driver [tsl2550] using legacy resume method
[ 0.712029] at24 1-0051: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.719931] Detected a daughter card on AM335x EVM..
[ 0.724991] at24 1-0050: 32768 byte 24c256 EEPROM, writable, 64 bytes/write
[ 0.740372] Board name: A33515BB
[ 0.743749] Board version: 1.1A
[ 0.747018] SKU: SKU#01
[ 0.750114] The board is general purpose EVM in profile 0
[ 0.756633] da8xx_lcdc da8xx_lcdc.0: GLCD: Found TFC_S9700RTWV35TR_01B panel
[ 0.777286] Console: switching to colour frame buffer device 100x30
[ 0.789709] TSC connected to beta GP EVM
[ 0.794924] omap_i2c.2: alias fck already exists
[ 0.812284] omap_i2c omap_i2c.2: bus 2 rev4.0 at 100 kHz
[ 0.818629] tsl2550 2-0039: standard operating mode
[ 0.824429] tsl2550 2-0039: support ver. 1.2 enabled
[ 0.830337] omap_hsmmc.0: alias fck already exists
[ 0.835801] omap_hsmmc.2: alias fck already exists
[ 0.841158] Configure Bluetooth Enable pin...
[ 0.845795] _omap_mux_get_by_name: Could not find signal gpmc_a8.gpio1_22
[ 0.854486] lis3lv02d: 8 bits 3DLH sensor found
[ 0.932625] input: ST LIS3LV02DL Accelerometer as /devices/platform/lis3lv02d/input/input0
[ 0.943524] mtdoops: mtd device (mtddev=name/number) must be supplied
[ 0.950414] omap2-nand driver initializing
[ 0.955112] ONFI flash detected
[ 0.958507] ONFI param page 0 valid
[ 0.962148] NAND device: Manufacturer ID: 0x2c, Chip ID: 0xda (Micron MT29F2G08ABAEAWP)
[ 0.970546] Creating 8 MTD partitions on "omap2-nand.0":
[ 0.976104] 0x000000000000-0x000000020000 : "SPL"
[ 0.982775] 0x000000020000-0x000000040000 : "SPL.backup1"
[ 0.989692] 0x000000040000-0x000000060000 : "SPL.backup2"
[ 0.996663] 0x000000060000-0x000000080000 : "SPL.backup3"
[ 1.003640] 0x000000080000-0x000000260000 : "U-Boot"
[ 1.010831] 0x000000260000-0x000000280000 : "U-Boot Env"
[ 1.017721] 0x000000280000-0x000000780000 : "Kernel"
[ 1.026171] 0x000000780000-0x000010000000 : "File System"
[ 1.135439] OneNAND driver initializing
[ 1.182252] davinci_mdio davinci_mdio.0: davinci mdio revision 1.6
[ 1.188701] davinci_mdio davinci_mdio.0: detected phy mask fffffffe
[ 1.195952] davinci_mdio.0: probed
[ 1.199500] davinci_mdio davinci_mdio.0: phy[0]: device 0:00, driver unknown
[ 1.207041] CAN device driver interface
[ 1.211036] CAN bus driver for Bosch D_CAN controller 1.0
[ 1.217432] usbcore: registered new interface driver cdc_ether
[ 1.223733] usbcore: registered new interface driver cdc_subset
[ 1.229954] Initializing USB Mass Storage driver...
[ 1.235244] usbcore: registered new interface driver usb-storage
[ 1.241502] USB Mass Storage support registered.
[ 1.246387] musb-hdrc musb-hdrc.1: MUSB HDRC host driver
[ 1.251995] musb-hdrc musb-hdrc.1: new USB bus registered, assigned bus number 1
[ 1.259832] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002
[ 1.266929] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[ 1.274467] usb usb1: Product: MUSB HDRC host driver
[ 1.279642] usb usb1: Manufacturer: Linux 3.1.0 musb-hcd
[ 1.285184] usb usb1: SerialNumber: musb-hdrc.1
[ 1.290714] hub 1-0:1.0: USB hub found
[ 1.294688] hub 1-0:1.0: 1 port detected
[ 1.299857] mousedev: PS/2 mouse device common for all mice
[ 1.306666] input: matrix-keypad as /devices/platform/matrix-keypad/input/input1
[ 1.315824] input: ti-tsc-adcc as /devices/platform/tsc/input/input2
[ 1.323615] Unhandled fault: external abort on non-linefetch (0x1028) at 0xf9e3e044
[ 1.331614] Internal error: : 1028 [#1]
[ 1.335611] Modules linked in:
[ 1.338802] CPU: 0 Not tainted (3.1.0 #1)
[ 1.343360] PC is at rtc_wait_not_busy+0x28/0x44
[ 1.348178] LR is at omap_rtc_read_time+0x18/0x68
[ 1.353085] pc : [<c02cbbbc>] lr : [<c02cbeac>] psr: 40000093
[ 1.353092] sp : cf81bce0 ip : cf81bcf8 fp : cf81bcf4
[ 1.365064] r10: cf81bd74 r9 : cf81bdd4 r8 : 00000000
[ 1.370512] r7 : cf81bd74 r6 : 00000000 r5 : c05f4528 r4 : 00000001
[ 1.377320] r3 : f9e3e000 r2 : cf81bd74 r1 : cf81bd74 r0 : 0001a36e
[ 1.384131] Flags: nZcv IRQs off FIQs on Mode SVC_32 ISA ARM Segment kernel
[ 1.391846] Control: 10c5387d Table: 80004019 DAC: 00000015
[ 1.397840] Process swapper (pid: 1, stack limit = 0xcf81a2f0)
[ 1.403925] Stack: (0xcf81bce0 to 0xcf81c000)
[ 1.408474] bce0: cf81bd74 cf3c2800 cf81bd0c cf81bcf8 c02cbeac c02cbba0 c02cbe94 cf3c295c
[ 1.417010] bd00: cf81bd2c cf81bd10 c02c9db0 c02cbea0 cf816b80 cf81bd74 cf3c2960 cf3c2800
[ 1.425545] bd20: cf81bd4c cf81bd30 c02ca24c c02c9d54 cf3c2800 cf3c2800 c058cb00 c04ba320
[ 1.434081] bd40: cf81bdcc cf81bd50 c02ca284 c02ca220 cf808740 00000000 c05f44f8 c058cb00
[ 1.442617] bd60: c04ba320 c058cb00 00000000 00000000 cf81bdb4 00000000 00000000 00000000
[ 1.451151] bd80: 00000000 00000000 00000000 00000000 00000000 00000000 000080d0 c04ba320
[ 1.459685] bda0: cf81bdfc cf3c2800 c05f44f8 c058cb00 c04ba320 00000000 00000000 c05afc80
[ 1.468220] bdc0: cf81be2c cf81bdd0 c02c95f8 c02ca26c c058cd34 c058cd34 cf81be2c cf81bde8
[ 1.476754] bde0: c0043924 c0043230 cf81be3c 00000000 cf816b80 c0035f14 00000000 00000000
[ 1.485289] be00: cf81be2c c058cd34 c05f4528 c058caf8 00000000 c058cb00 00000000 cf3c18c0
[ 1.493823] be20: cf81be5c cf81be30 c0556038 c02c9488 00000000 cf81be40 c058cb00 c05f2fb0
[ 1.502357] be40: c05be328 c05afc44 00000000 c0555e58 cf81be6c cf81be60 c02313d0 c0555e88
[ 1.510892] be60: cf81be9c cf81be70 c022fee4 c02313bc cf81be9c cf81be80 c02317b0 c058cb00
[ 1.519427] be80: c05afc44 c058cb34 00000000 00000000 cf81bebc cf81bea0 c02300c4 c022fd88
[ 1.527962] bea0: c0230030 c05afc44 c0230030 00000000 cf81bee4 cf81bec0 c022eda0 c023003c
[ 1.536496] bec0: cf806ef8 cf891b70 c01d1a1c c05afc44 c05a4598 cf3c4a40 cf81bef4 cf81bee8
[ 1.545031] bee0: c022fa34 c022ed54 cf81bf24 cf81bef8 c022f6a0 c022fa1c c04ba320 cf81bf08
[ 1.553567] bf00: c05afc44 c056ca28 cf81a000 00000000 00000000 c0555e58 cf81bf4c cf81bf28
[ 1.562102] bf20: c0230668 c022f510 c023140c c05afc30 c056ca28 cf81a000 00000000 00000000
[ 1.570637] bf40: cf81bf5c cf81bf50 c02318a8 c02305f4 cf81bf74 cf81bf60 c02318cc c0231858
[ 1.579172] bf60: 00000000 c05c2dc0 cf81bf84 cf81bf78 c0555e78 c02318b8 cf81bfdc cf81bf88
[ 1.587707] bf80: c0008794 c0555e64 c0075b1c c00f486c 0000007f c00f46e8 cf81bfbc 3231bea0
[ 1.596243] bfa0: 00000037 00000000 cf81bfc4 0000018c c059a934 c056c8f0 c056ca28 c004076c
[ 1.604778] bfc0: 00000013 00000000 00000000 00000000 cf81bff4 cf81bfe0 c0534884 c0008764
[ 1.613313] bfe0: 00000000 c05347e8 00000000 cf81bff8 c004076c c05347f4 c00300c8 00060aaa
[ 1.621841] Backtrace:
[ 1.624403] [<c02cbb94>] (rtc_wait_not_busy+0x0/0x44) from [<c02cbeac>] (omap_rtc_read_time+0x18/0x68)
[ 1.634113] r5:cf3c2800 r4:cf81bd74
[ 1.637855] [<c02cbe94>] (omap_rtc_read_time+0x0/0x68) from [<c02c9db0>] (__rtc_read_time.clone.9+0x68/0x6c)
[ 1.648108] r4:cf3c295c r3:c02cbe94
[ 1.651847] [<c02c9d48>] (__rtc_read_time.clone.9+0x0/0x6c) from [<c02ca24c>] (rtc_read_time+0x38/0x4c)
[ 1.661646] r5:cf3c2800 r4:cf3c2960
[ 1.665385] [<c02ca214>] (rtc_read_time+0x0/0x4c) from [<c02ca284>] (__rtc_read_alarm+0x24/0x33c)
[ 1.674639] r7:c04ba320 r6:c058cb00 r5:cf3c2800 r4:cf3c2800
[ 1.680562] [<c02ca260>] (__rtc_read_alarm+0x0/0x33c) from [<c02c95f8>] (rtc_device_register+0x17c/0x28c)
[ 1.690563] [<c02c947c>] (rtc_device_register+0x0/0x28c) from [<c0556038>] (omap_rtc_probe+0x1bc/0x3fc)
[ 1.700377] [<c0555e7c>] (omap_rtc_probe+0x0/0x3fc) from [<c02313d0>] (platform_drv_probe+0x20/0x24)
[ 1.709912] [<c02313b0>] (platform_drv_probe+0x0/0x24) from [<c022fee4>] (driver_probe_device+0x168/0x2b4)
[ 1.719990] [<c022fd7c>] (driver_probe_device+0x0/0x2b4) from [<c02300c4>] (__driver_attach+0x94/0x98)
[ 1.729697] r8:00000000 r7:00000000 r6:c058cb34 r5:c05afc44 r4:c058cb00
[ 1.736713] [<c0230030>] (__driver_attach+0x0/0x98) from [<c022eda0>] (bus_for_each_dev+0x58/0x84)
[ 1.746058] r6:00000000 r5:c0230030 r4:c05afc44 r3:c0230030
[ 1.751980] [<c022ed48>] (bus_for_each_dev+0x0/0x84) from [<c022fa34>] (driver_attach+0x24/0x28)
[ 1.761143] r6:cf3c4a40 r5:c05a4598 r4:c05afc44
[ 1.765974] [<c022fa10>] (driver_attach+0x0/0x28) from [<c022f6a0>] (bus_add_driver+0x19c/0x26c)
[ 1.775146] [<c022f504>] (bus_add_driver+0x0/0x26c) from [<c0230668>] (driver_register+0x80/0x144)
[ 1.784500] [<c02305e8>] (driver_register+0x0/0x144) from [<c02318a8>] (platform_driver_register+0x5c/0x60)
[ 1.794662] r8:00000000 r7:00000000 r6:cf81a000 r5:c056ca28 r4:c05afc30
[ 1.801485] r3:c023140c
[ 1.804226] [<c023184c>] (platform_driver_register+0x0/0x60) from [<c02318cc>] (platform_driver_probe+0x20/0x70)
[ 1.814849] [<c02318ac>] (platform_driver_probe+0x0/0x70) from [<c0555e78>] (rtc_init+0x20/0x24)
[ 1.824013] r4:c05c2dc0 r3:00000000
[ 1.827756] [<c0555e58>] (rtc_init+0x0/0x24) from [<c0008794>] (do_one_initcall+0x3c/0x180)
[ 1.836477] [<c0008758>] (do_one_initcall+0x0/0x180) from [<c0534884>] (kernel_init+0x9c/0x130)
[ 1.845570] [<c05347e8>] (kernel_init+0x0/0x130) from [<c004076c>] (do_exit+0x0/0x6a0)
[ 1.853827] r5:c05347e8 r4:00000000
[ 1.857566] Code: e5953000 e30a036e e3400001 e2844001 (e5d33044)
[ 1.864043] ---[ end trace 38fd4428f262a81d ]---
[ 1.868874] Kernel panic - not syncing: Attempted to kill init!
[ 1.875062] Backtrace:
[ 1.877642] [<c0017990>] (dump_backtrace+0x0/0x110) from [<c03e6c7c>] (dump_stack+0x18/0x1c)
[ 1.886457] r6:c058f870 r5:c058f870 r4:c05c3da0 r3:c058e250
[ 1.892393] [<c03e6c64>] (dump_stack+0x0/0x1c) from [<c03e6cec>] (panic+0x6c/0x1a0)
[ 1.900393] [<c03e6c80>] (panic+0x0/0x1a0) from [<c0040d30>] (do_exit+0x5c4/0x6a0)
[ 1.908297] r3:cf816da0 r2:cf81bb34 r1:cf81bb34 r0:c04bd830
[ 1.914226] r7:cf816b80
[ 1.916875] [<c004076c>] (do_exit+0x0/0x6a0) from [<c0017dc8>] (die+0x270/0x2bc)
[ 1.924597] r7:cf81bba2
[ 1.927248] [<c0017b58>] (die+0x0/0x2bc) from [<c0017e34>] (arm_notify_die+0x20/0x58)
[ 1.935432] [<c0017e14>] (arm_notify_die+0x0/0x58) from [<c0008584>] (do_DataAbort+0x9c/0xa0)
[ 1.944353] [<c00084e8>] (do_DataAbort+0x0/0xa0) from [<c0013d98>] (__dabt_svc+0x38/0x60)
[ 1.952894] Exception stack(0xcf81bc98 to 0xcf81bce0)
[ 1.958163] bc80: 0001a36e cf81bd74
[ 1.966709] bca0: cf81bd74 f9e3e000 00000001 c05f4528 00000000 cf81bd74 00000000 cf81bdd4
[ 1.975257] bcc0: cf81bd74 cf81bcf4 cf81bcf8 cf81bce0 c02cbeac c02cbbbc 40000093 ffffffff
[ 1.983796] r8:00000000 r7:cf81bccc r6:ffffffff r5:40000093 r4:c02cbbbc
[ 1.990818] [<c02cbb94>] (rtc_wait_not_busy+0x0/0x44) from [<c02cbeac>] (omap_rtc_read_time+0x18/0x68)
[ 2.000537] r5:cf3c2800 r4:cf81bd74
[ 2.004295] [<c02cbe94>] (omap_rtc_read_time+0x0/0x68) from [<c02c9db0>] (__rtc_read_time.clone.9+0x68/0x6c)
[ 2.014558] r4:cf3c295c r3:c02cbe94
[ 2.018299] [<c02c9d48>] (__rtc_read_time.clone.9+0x0/0x6c) from [<c02ca24c>] (rtc_read_time+0x38/0x4c)
[ 2.028108] r5:cf3c2800 r4:cf3c2960
[ 2.031848] [<c02ca214>] (rtc_read_time+0x0/0x4c) from [<c02ca284>] (__rtc_read_alarm+0x24/0x33c)
[ 2.041104] r7:c04ba320 r6:c058cb00 r5:cf3c2800 r4:cf3c2800
[ 2.047030] [<c02ca260>] (__rtc_read_alarm+0x0/0x33c) from [<c02c95f8>] (rtc_device_register+0x17c/0x28c)
[ 2.057021] [<c02c947c>] (rtc_device_register+0x0/0x28c) from [<c0556038>] (omap_rtc_probe+0x1bc/0x3fc)
[ 2.066832] [<c0555e7c>] (omap_rtc_probe+0x0/0x3fc) from [<c02313d0>] (platform_drv_probe+0x20/0x24)
[ 2.076368] [<c02313b0>] (platform_drv_probe+0x0/0x24) from [<c022fee4>] (driver_probe_device+0x168/0x2b4)
[ 2.086445] [<c022fd7c>] (driver_probe_device+0x0/0x2b4) from [<c02300c4>] (__driver_attach+0x94/0x98)
[ 2.096153] r8:00000000 r7:00000000 r6:c058cb34 r5:c05afc44 r4:c058cb00
[ 2.103171] [<c0230030>] (__driver_attach+0x0/0x98) from [<c022eda0>] (bus_for_each_dev+0x58/0x84)
[ 2.112517] r6:00000000 r5:c0230030 r4:c05afc44 r3:c0230030
[ 2.118435] [<c022ed48>] (bus_for_each_dev+0x0/0x84) from [<c022fa34>] (driver_attach+0x24/0x28)
[ 2.127599] r6:cf3c4a40 r5:c05a4598 r4:c05afc44
[ 2.132435] [<c022fa10>] (driver_attach+0x0/0x28) from [<c022f6a0>] (bus_add_driver+0x19c/0x26c)
[ 2.141598] [<c022f504>] (bus_add_driver+0x0/0x26c) from [<c0230668>] (driver_register+0x80/0x144)
[ 2.150956] [<c02305e8>] (driver_register+0x0/0x144) from [<c02318a8>] (platform_driver_register+0x5c/0x60)
[ 2.161118] r8:00000000 r7:00000000 r6:cf81a000 r5:c056ca28 r4:c05afc30
[ 2.167944] r3:c023140c
[ 2.170685] [<c023184c>] (platform_driver_register+0x0/0x60) from [<c02318cc>] (platform_driver_probe+0x20/0x70)
[ 2.181306] [<c02318ac>] (platform_driver_probe+0x0/0x70) from [<c0555e78>] (rtc_init+0x20/0x24)
[ 2.190472] r4:c05c2dc0 r3:00000000
[ 2.194218] [<c0555e58>] (rtc_init+0x0/0x24) from [<c0008794>] (do_one_initcall+0x3c/0x180)
[ 2.202937] [<c0008758>] (do_one_initcall+0x0/0x180) from [<c0534884>] (kernel_init+0x9c/0x130)
[ 2.212010] [<c05347e8>] (kernel_init+0x0/0x130) from [<c004076c>] (do_exit+0x0/0x6a0)
[ 2.220269] r5:c05347e8 r4:00000000