i build a new RTSC project in CCS5. after adding the source code " cpsw_singlecore.c " in the folder <...>\pdk_C6678_1_0_0_17\packages\ti\drv\pa\example\emacExample. when i want to build it, it shows "error: unresolved symbols remain" in console as showed ? what's the problem?
**** Build of configuration Debug for project TryNet ****
C:\Program Files\Texas Instruments\ccsv5\utils\gmake\gmake -k all
'Building target: TryNet.out'
'Invoking: C6000 Linker'
"C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/bin/cl6x" -mv6600 -g --diag_warning=225 --abi=eabi -z -m"TryNet.map" --warn_sections -i"C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/lib" -i"C:\Program Files\Texas Instruments\pdk_C6678_1_0_0_17\packages\ti\drv\pa\lib" -i"C:\Program Files\Texas Instruments\pdk_C6678_1_0_0_17\packages\ti\csl\lib" -i"C:\Program Files\Texas Instruments\pdk_C6678_1_0_0_17\packages\ti\platform\evmc6678l\platform_lib\lib\debug" -i"C:/Program Files/Texas Instruments/ccsv5/tools/compiler/c6000/include" --reread_libs --rom_model -o "TryNet.out" -l"./configPkg/linker.cmd" "./cpsw_singlecore.obj" -l"libc.a" -l"C:\Program Files\Texas Instruments\pdk_C6678_1_0_0_17\packages\ti\drv\pa\lib\ti.drv.pa.ae66" -l"C:\Program Files\Texas Instruments\pdk_C6678_1_0_0_17\packages\ti\platform\evmc6678l\platform_lib\lib\debug\ti.platform.evm6678l.ae66" -l"C:\Program Files\Texas Instruments\pdk_C6678_1_0_0_17\packages\ti\csl\lib\ti.csl.ae66" -l"C:\Program Files\Texas Instruments\pdk_C6678_1_0_0_17\packages\ti\csl\lib\ti.csl.intc.ae66" "../cpsw_linker.cmd"
<Linking>
undefined first referenced
>> Compilation failure
symbol in file
--------- ----------------
CycleDelay ./cpsw_singlecore.obj
Init_Cppi ./cpsw_singlecore.obj
Init_Cpsw ./cpsw_singlecore.obj
Init_PASS ./cpsw_singlecore.obj
Init_Qmss ./cpsw_singlecore.obj
SendPacket ./cpsw_singlecore.obj
Setup_PASS ./cpsw_singlecore.obj
Setup_Rx ./cpsw_singlecore.obj
Setup_Tx ./cpsw_singlecore.obj
gRxCounter ./cpsw_singlecore.obj
gTxCounter ./cpsw_singlecore.obj
view_ale_table ./cpsw_singlecore.obj
error: unresolved symbols remain
error: errors encountered during linking; "TryNet.out" not built