This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Start address is covered by existing entry, can not create TLB entry for address



root@beagleboard:/opt/dvsdk/omap3530# ./decode -v davincieffect_ntsc_1.m2v
Decode demo started.
[ 2071.503936] Start address is covered by existing entry, can not create TLB entry for address: [0x86300000]
size: [0x100000]
[ 2071.515258]  DSP_init status [0x80008050]
Error: Failed to open codec engi[ 2071.523162] Start address is covered by existing entry, can not create TLB
entry for address: [0x86300000] size: [0x100000]
ne decode
[ 2071.534729]  DSP_init status [0x80008050]
Error: Failed to open codec engine decode

mode "480x640-56"
        # D: 24.685 MHz, H: 38.571 kHz, V: 55.900 Hz
        geometry 480 640 640 400 32
        timings 40510 40 2[ 2071.571838] cannot enable LCD, DVI is enabled
4 39 9 96 2
        accel false
        rgba 8/16,8/8,8/0,0/0
endmode