Part Number: AM6422
Other Parts Discussed in Thread: TMDS64EVM
Hi,
I copied, latest SYSFW (sysfw_hs_fs_signed.h, sysfw-hs-enc.bin, sysfw-hs-enc-cert.bin, sysfw-hs-fs-enc.bin, sysfw-hs-fs-enc-cert.bin) from version 12.01.00.33. I took these file from 12.01.00.33.
Then, I copy paste, overwrite the same one in 09_01_00_41.
Then, I rebuild and recompilaiton and running at TMDS64EVM.
you will find dev boot mode doesn't work at more, the original example of
C:\ti\mcu_plus_sdk_am64x_09_01_00_41\examples\drivers\sciclient\sciclient_ccs_init\am64x-evm
not running anymore.
question, is there any difference between the two? either the way communicate with dmsc, or driver, clock, resource manager, power manager,
eg: would you list all difference?
What is the safest way to update SYSFW, we would like to keep the same code as old version.
Thanks