This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

how many DM8148 EZSDK OpenMax VFPC DEI is support?



I know DM8148 EZSDK OpenMax VFPC DEI  has at most two input and two output.

I want to use more than one DEI, so, 

1. how many DEI component is support in DM8148.  if more than one is support, Should I use different handle, or one handle but different port?

   from the manual, It seems that only one DEI is support, which have two outpu.

 

 I think the number of component is depend on hardware. and DM8148 only have two SC hardware. so only one DEI is support.


But the handle can be created multi-times, the multi-DEI is running in serial.

2.how many SC commonent is support in DM8148?  if more than one is support, Should I use different handle, or one handle but different port?

  3. how to make output port of comonent A connect input port of two diffent component.

    OR can I split output, half to B and half to C.

    OR I change the VLPB to copy buffer. this way, the buffer is copied and waste time and resources.

    I am using DEI to do this, so I need more than DEI to work