AM62A7-Q1: EMMC part compatibility

Part Number: AM62A7-Q1
Other Parts Discussed in Thread: SK-AM62A-LP

Please confirm the list of compatible eMMC manufacturers. I have shortlisted few parts for my requirement and willing to confirm the same through private channel/chat.

 

Thanks,

Nikunj

  • Hello Nikunj,

    Thank you for your query !

    TI does NOT not maintain a compatible memory list and validation has been done using the memory chip on the TI SITARA processor corresponding EVM(s).

    You should refer to the manufacturer for more info on any memory chip specific performance, parameters, commands, etc.

    The AM62A MMC0 eMMC host controller support is validated for the eMMC NAND flashes available on the SK-AM62A-LP EVM board.

    Here is the SK-AM62A-LP Design Package Folder and Files List where you can find the validated eMMC components listed:

    Design File Package Rev.B of the SK-AM62A-LP:

    https://www.ti.com/lit/zip/sprr491

    Design File package Rev.C - E1,E2,E3 of the SK-AM62A-LP:

    https://www.ti.com/lit/zip/SPRR459

    So validated to operate correctly on the SK-AM62A-LP (check SK-AM62A-LP Evaluation board | TI.com) are the Micron's eMMC NAND Flash memories:

    The 256Gb (32GB) MTFC32GAZAQHD-IT (used in the older rev.B)

    The 128Gb (16GB) MTFC16GAPALBH-IT (used in Rev.C-E1,E2,E3)

    I hope this answers your question.

    Best Regards,

    Anastas Yordanov 

  • Hello,

    The eMMC controller is compliant to JEDEC 5.1 so as long as the eMMC card is compliant to the same standard everything should work as expected with the latest SDKs.