This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using IMGLIB. How can I do?



Hi.

To use IMGLIB is necessary to say that CCS is right?

2.2.1 Looking at spruf30a without CCS looks like it could be the link, right?

When I use IMGLIB if I really need that CCS.

I try study CCS.

But I think 2.2.1 in spruf30a(IMGLIB docs) looks like I can compile and link without CCS.

Is imglib2.l64p necessary in order to work with dsp?

I want know  in detail 2.2.1.

"cl6x main.c -z -o IMG_boundary_drv.out -lrts64plus.lib -limglib2.l64P"

I have trouble with to add the sentence in upper line to which 'Makefile' located at and where to use 'make'.

I want know method.(link and make).

Please answer for my answer in detail, plz.

Thank you.