Other Parts Discussed in Thread: ALP
Respected Sir/Madam,
I am using Centaurus board(TMDXEVM8148 ALP). WHen i try to connect to the Cortex A8 processor, after loading GEL files, it stops at msg on consol:
Centaurus USB_PLL Init is in Progress, Please wait............
or some times it stops at msg:
PRCM for EMIF0, EMIF1 and DMM are in Progress, Please wait...........
and then i got this error:
CortexA8: The GEL callback "OnTargetConnect()" is no longer running atomically
is it GEL files problem or something wrong ? Please help me.
I am using CCS v 4.2.2.00033 and i am using spectrum digital's XDS 510 USB JTAG. i am attaching my gel files also:
8015.Copy of New_Centaurus_20Mhz_Si.txt
//Created by Shreyas Prasad (shreyasp@ti.com)
#define PRCM_BASE_ADDR 0x48180000
#define WR_MEM_32(addr, data) *(unsigned int*)(addr) =(unsigned int)(data)
#define RD_MEM_32(addr) *(unsigned int*)(addr)
#define UWORD32 unsigned int
#define CM_ALWON_SPINBOX_CLKCTRL (PRCM_BASE_ADDR + 0x1598)
#define CM_ALWON_MAILBOX_CLKCTRL (PRCM_BASE_ADDR + 0x1594)
#define CM_ALWON_L3_SLOW_CLKSTCTRL (PRCM_BASE_ADDR + 0x1400)
hotmenu enableSpinlocks()
{
GEL_TextOut("\tPRCM for spinlock Initialization in Progress \n","Output",1,1,1);
WR_MEM_32(CM_ALWON_L3_SLOW_CLKSTCTRL, 2);
WR_MEM_32(CM_ALWON_SPINBOX_CLKCTRL, 2);
/* Wait for IDLEST to read 0x0 indicating that the module is fully functional */
while(((RD_MEM_32(CM_ALWON_SPINBOX_CLKCTRL)&0x30000)>>16)!=0);
GEL_TextOut("\tspinlock Accesses are PASSED \n","Output",1,1,1);
GEL_TextOut("\tspinlock Initialization in Done \n","Output",1,1,1);
}
hotmenu enableMaiboxes()
{
GEL_TextOut("\tPRCM for mailboxes Initialization in Progress \n","Output",1,1,1);
WR_MEM_32(CM_ALWON_L3_SLOW_CLKSTCTRL, 2);
WR_MEM_32(CM_ALWON_MAILBOX_CLKCTRL, 2);
/* Wait for IDLEST to read 0x0 indicating that the module is fully functional */
while(((RD_MEM_32(CM_ALWON_MAILBOX_CLKCTRL)&0x30000)>>16)!=0);
GEL_TextOut("\tmailboxes Accesses are PASSED \n","Output",1,1,1);
GEL_TextOut("\tPmailboxes Initialization in Done \n","Output",1,1,1);
}
OnTargetConnect()
{
GEL_LoadGel("$(GEL_file_dir)\\New_Centaurus_20MHz_Si.gel");
GEL_TextOut("--->>> Starting A8 <<<---\n");
DucatiClkEnable();
GEMSSClkEnable();
Unlock_PLL_Control_MMR();
ControlModule_ClkEnable();
PLL_CLOCKS_Config();
//PrcmAlwayOnClkEnable(); //does not come out of loop
DDR2_Initialization();
//L3_PLL_Config();
//SATA_PLL_Config();
Ethernet_PinMux_Setup();
enableMaiboxes();
enableSpinlocks();
}
Thanks in advance.