This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problems using Accesing pixels in a frame on the DM6437



Hello.

I've just start with Accessing Pixels in a Frame on the DM643x  in my evmDM6437.

I think is the best project to probe an sobel edge detection, but I have problems. I would like to create another "frameBuffPtr" (named "frameBuffPtrOut") where putting my proccessed pixels. For that, I define:

  PSP_VPSSSurfaceParams *frameBuffPtrOut;

And in the first step I do is transfering pixels from original buffer to this second buffer:

    for (i=0;i<ROWS_IMAGE_IN;i++)
    {
        for (j=0;j<COLS_IMAGE_IN*2;j++)
        {
            *((unsigned char*)frameBuffPtrOut->frame.frameBufferPtr+i*COLS_IMAGE_IN*2+j)=
            *((unsigned char*)frameBuffPtr->frame.frameBufferPtr+i*COLS_IMAGE_IN*2+j);
        }
        
    }

where ROWS_IMAGE=480 and COLS_IMAGE_IN=720

After that, I change some parameters in function calls to represent this second buffer in output video signal

    BCACHE_wbInv((void*)(frameBuffPtrOut->frame.frameBufferPtr), ROWS_IMAGE_IN*COLS_IMAGE_IN*2, 1);

    /* display the video frame */
    FVID_exchange(hGioVpbeVid0, &frameBuffPtrOut);

But I don't see anything. I put a breakpoint and I surprised because this second buffer is located at address 0!!

How anyone why this happens? I think this variable/buffer would be allocated after 0x80000000 where DDR2 is defined.

Do I need to do some changes in .tcf configuration?

Thanks a lot