Other Parts Discussed in Thread: TMS320DM6437
Hi
I have TMS320DM6437 EVM and I have a little problem with launch Demo. Unfortunately I have no experience with any DSP. If I get board I first tried launch demo in stand-alone mode and all worked done (on output screen I have seen input signal from camera). When I erased flash memory and load the same program dm6437_demo.hex in FlashBurn DSK to memory (CCS -> connect -> FlasBurn DSK -> erase flash -> program flash -> close -> disconnect) and turned the board on Demo didn´t run (I didn´t see any signal on output).
I also tried run program in CCS (CCS -> connect -> open project -> dm6437_demo.pjt -> rebuild all -> load program -> go main) and it showed „running“ but board didn‘t work (I didn´t see any signal on output).
Can you tell me what I do wrong?
I use CCS_v3.3, dvsdk_1_01_00_15 and FlashBurn DSK 3.11
Thanks
Tomas Reichl