AM6421: Ethernet-IP

Part Number: AM6421

Hi

      we are using Industrialsdk ind_comms_sdk_am64x_11_00_00_13 version on AM6421

 

 We have taken the Ethernet-ip stack  discrete_io_device example given in sdk.

 

  With the given 

#define CFG_PROFILE_DIO_DEVICE_ASSEMBLY_PRODUCING     DIO_DEVICE_ASM_4_Input_Point_No_Status /*!< Producing Assembly Instance */
#define CFG_PROFILE_DIO_DEVICE_ASSEMBLY_CONSUMING     DIO_DEVICE_ASM_4_Output_Point     //DIO_DEVICE_ASM_4_Output_Point /*!< Consuming Assembly Instance */
#define CFG_PROFILE_DIO_DEVICE_ASSEMBLY_CONFIGURATION DIO_DEVICE_ASM_Output_Configuration /*!< Configuration Assembly Instance */

#define CFG_PROFILE_DIO_DEVICE_DOP_NUM_OF_INST        4 /*!< Number of instances of Discrete Output Point Object */
#define CFG_PROFILE_DIO_DEVICE_DIP_NUM_OF_INST        4  /*!< Number of instances of Discrete Input Point Object */

 

    The device is working fine.

 

But when we change DIO_DEVICE_ASM_4_Output_Point  to DIO_DEVICE_ASM_8_Output_Point

The device is not working and basic ping is failing.

 Can you please confirm if DIO_DEVICE_ASM_8_Output_Point  works.

we have used the same exaple code given in SDK.