Part Number: AM625
Other Parts Discussed in Thread: SK-AM62B-P1
Hi,
We are working with the SK-AM62B-P1 and the QNX SDK.
We have also integrated the PSDK to the BSP and built the IFS and the TI Filessystem
We are able to boot the board successfully but on loding the cpsw driver, we see error on the log.
`devs-smsc.so: loaded
Jan 01 00:18:25.430 io_sock.1040403 main_buffer 28 devs-cpsw-am62x.so: loading module with ""
Jan 01 00:18:25.436 io_sock.1040403..0 stderr* 0 unknown symbol: miibus_devclass referenced from devs-cpsw-am62x.so
Jan 01 00:18:25.436 io_sock.1040403..0 stderr 0 unknown symbol: etherswitch_devclass referenced from devs-cpsw-am62x.so
Jan 01 00:18:25.437 io_sock.1040403 main_buffer 28 link_elf_load_file: devs-cpsw-am62x.so load fail cause:Unresolved symbol
Jan 01 00:18:25.446 io_sock.1040403 main_buffer 28 devs-cpsw-am62x.so: module not loaded, error 8
Jan 01 00:18:25.446 io_sock.1040403 main_buffer 28 devs-cpsw-am62x.so: scheduled for removal
Jan 01 00:18:25.446 io_sock.1040403 main_buffer 28 devs-cpsw-am62x.so: failed to mount (8) Exec format error
Jan 01 00:18:25.446 io_sock.1040403 main_buffer 28 devs-cpsw-am62x.so: module removed
The command sequence to load the driver is:
sh -c "isend -n/dev/i2c1 -a0x23 0x0e > /dev/null 2>&1"
sh -c "isendrecv -n /dev/i2c1 -a0x23 -l1 > /dev/null 2>&1"
sh -c "isend -n/dev/i2c1 -a0x23 0x0e 0xf3 > /dev/null 2>&1"
sh -c "isend -n/dev/i2c1 -a0x23 0x0e > /dev/null 2>&1"
sh -c "isendrecv -n /dev/i2c1 -a0x23 -l1 > /dev/null 2>&1"
sh -c "isend -n/dev/i2c1 -a0x23 0x06 > /dev/null 2>&1"
sh -c "isendrecv -n /dev/i2c1 -a0x23 -l1 > /dev/null 2>&1"
sh -c "isend -n/dev/i2c1 -a0x23 0x06 0xff > /dev/null 2>&1"
sh -c "isend -n/dev/i2c1 -a0x23 0x06 > /dev/null 2>&1"
sh -c "isendrecv -n /dev/i2c1 -a0x23 -l1 > /dev/null 2>&1"
io-sock -m phy -m usb -d axe -d axge -d cdce -d smsc -mfdt -dcpsw-am62x
Let us know how to enable the ethernet on the starterkit and connect to the host via qconn.
Regards,
Surendrakumar