Figure 3-1 of sprs659e shows SARAM size as 200K. Everywhere else in the datasheet it's stated to be 192K. Which is correct?
The block size of the External-CS0 space is shown as 8M minus 264K, yet the byte addresses are 800000h - 50000h which is 8M minus 320K.