This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

How does " --C6Run:replace_malloc" works? a question on C6runlib

hi,

The c6runlib documents say  " --C6Run:replace_malloc" can be used when calling c6runlib-ar so that arm-side buffers  can be shared with the DSP.

For example, I have three C source codes like  main.c,arm.c, dsp.c.  I want dsp.c run on dsp. 

so I call c6runlib-cc to compile dsp.c to dsp.o.  Then I call c6runlib-ar to create an arm static library  dsp.lib from dsp.o.

But what I can't understand is , c6runlib-ar only affects dsp.o so option " --C6Run:replace_malloc" only replaces malloc-like api in the code dsp.c. 

How can it replace memory allocations in code main.c and arm.c ? 

I must misunderstand  C6runlib mechanism.How can I learn in detail how c6run works about data and address passing between arm and dsp cores?

Thank you.

Francis.