This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

GenCodecPkg not supporting CCS5?

Hello,

I am trying to create a Universtal algorithm by running the GenCodecPkg wizard with CCS5.1.0.09. The package is generated and I can compile from the command window/gmake. But the CCS project doesn't not show up in the Project Explorer after it was imported as Existing CCS/CCE Eclipse Project (no error message from CCS). I followed http://processors.wiki.ti.com/index.php/Codec_Engine_GenCodecPkg_Wizard_FAQ#Create_an_XDM_Algorithm_and_Codec_Package as well as the iUniversal Lab Exercise procedure (Lab13a) in the training book from my co-worker who didn't use CCS5 in the triaining.

I am using CE codec_engine_2_26_01_09 and xdais_6_26_01_03 in the release DVSDK dvsdk_wince_01_11_00_03_patch_01. A couple of screenshots are attached.

Thanks,

Ying

screenshots1.doc