This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART Runnig at max speed

Hi everybody,

Can I use only  UART_TX and UART_RX to run at 4Mbps on DM814?

I do not need  to use CTS and RTS for this speed ?

Regards