I am currently using a Beagleboard-like design on a custom PCB. I am NOT using any USB ports, just an ethernet port. The Beagleboard design calls for the LAN9514 to handle communications from multiple USB ports and the ethernet port. It then feeds the upstream data THRU an USB3320 USB transceiver into the DM3730.
The Beagleboard also uses the ULPI port on the TPS65950 to handle a separate USB OTG port.
My question is thus: If I do not want to use the USB3320 can I route the upstream data from the LAN9514 directly into the ULPI port on the TPS65950?? Again, I am not using any USB ports in my design.