This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about VRAM setting in dm8168

After looking "TMS320DM81XX Graphics Control Using Frame Buffer Driver.pdf", I have a question about the following description

Given below are the basic steps to open FBDev nodes and draw GUI in display.
1) Boot kernel with at least 16M VRAM size.   ==> why there's a limitation in VRAM about 16M??

Any one know that?

  • Hi,

    This is because by default when ti81xxfb.ko is inserted it allocates buffer for 1920X1080 resolution and it requires almost 16MB for that buffer. Buffer is allocated using this VRAM memory.

    Regards,

    Hardik Shah

  • Thanks. Hardik.
    1. can you caculate the value of 16M? 1920x1080x2x3(3 graphic layer) ?? how did you get the value?
    2. if the limitation is at lease 16M, why did you set vram=40M in the document? 40M-16M=24M. What's the usage of 24M?

  • Please see my comments below.

    Regards,

    yihe

    Medwin Tsai said:

    Thanks. Hardik.
    1. can you caculate the value of 16M? 1920x1080x2x3(3 graphic layer) ?? how did you get the value?

    [yihe] 16M = 1920x1080*4(1 ARGB32 1080P buffer) * 2(2 such buffer)
    2. if the limitation is at lease 16M, why did you set vram=40M in the document? 40M-16M=24M. What's the usage of 24M?

    [yihe] there are three fbdev drivers, two HD and one SD, the 24 is for the second HD and SD framebuffer.