AM6548: AM6548 EUCRA support

Part Number: AM6548
Other Parts Discussed in Thread: AM6546, TMDX654IDKEVM

Hi Ti,

 

We are using AM6548 for our product. We are using ti-rt-linux-5.10.y, the commit id version is 101d44260b8dfbab27763581e4bbd534dd36ae33.

Now, due to EU CRA event, we want to know if there is LTS version for AM6548?

Also, including PRU firmware. It's related to kernel, right?

 

Eric

 

  • Hello Eric,

    Is there a particular part of CRA requirements which you are curious about?

    The PRU firmware was written and tested with the specific kernel version of the specific SDK. We suggest using the version of PRU firmware in the ti-linux-firmware repo which has been tagged with the same tag as the specific SDK that is being used: https://github.com/TexasInstruments/ti-linux-firmware/tree/ti-linux-firmware/ti-pruss

    If you change the Linux version, you would want to change to using the PRU firmware binaries which were tested with that Linux kernel version

    I am sending your thread to another team member to discuss the question about an LTS version of AM65x RT Linux.

    Regards,

    Nick

  • Hi Nick,

    Yes, because of EUCRA, we want to know if TI has an LTS version of the AM6548 kernel. If there is an LTS version and TI continues to support it, then we can consider upgrading to that version.

    Because the PRU firmware and kernel version are also dependent.

    If the kernel has an LTS version, then theoretically, wouldn't the PRU also have an LTS version?

    Eric

  • Hello Eric,

    The team member I sent you to was out of office, so I'm routing you to a third team member. Please ping the thread if you do not get a response within a day or so.

    I am not currently aware of an official "LTS version" of existing AM65x software. Our "typical" support strategy is to answer design questions about an official TI Linux SDK release for about 2 years after the SDK is released. But I might be unaware of an existing resource, and (like many companies) we are still figuring out all the effort required from our side to comply with the EU's CRA rules. The last time I checked in we were still waiting for the EU to decide specific details of CRA, but it has been a while since I looked into this myself. Hopefully those details are decided soon (if not already figured out), since it will take time for all of us to act based on those regulations.

    Regards,

    Nick

  • Hi Eric, 

    thank you for reaching out! We typically provide annual LTS SDK refreshes, with each release supported by our apps team for one year. 

    For AM65X specifically, design support is currently limited as outlined on our product support page: https://www.ti.com/product/AM6548

    I can check internally whether the AM65x SDK has received its LTS refresh this year or if one is still pending and share any available information.

    For additional information on TI's approach to the EU CRA, please refer to our CRA webpage: Cyber Resilience Act (CRA) | TI.com

    Hope this helps.

    Take care,

    Riya

  • On LTS refresh:

    Yes a refresh is planned as part our LTS commitment across this processor class. SDK release is scheduled at end of 4Q similar to 11.02 month/date.

    It will be with kernel 6.18, yocto wrynose as baseline.

    What is available already is CICD releases since many months.

    If you have any early development need, you can always take CICD snapshots and associated src repo tags.

    Ref: software-dl.ti.com/.../index.html

  • Hi,

    So, just to confirm, there will be an LTS release supported by late 2026, correct?

    Does Ti support it at least 5 years?

    Furthermore, I would like to inquire whether this support extends to the specific model we are using, AM6546BACDXA.

    We need to evaluate the feasibility of this upgrade. However, a colleague of mine previously asked about the AM6546, and it seems TI has limit support.

     

    btw, is the LTS version release by late 2026 is based on 11_02_05_02 SDK?

    Eric

  • Yes, end of 2026 there will be a LTS release and will be called as 12.02.xx.yy.zz

    11.02 is scarthgap and 6.12 kernel whereas next release shall be 6.18 kernel and yocto.

    Like every year, we shall evaluate and release a release end of next year based on future LTS kernel.

    We will validate on www.ti.com/.../TMDX654IDKEVM 

  • Hi Eric 

    To clarify on your 5-year question — as of now our typical support model for Sitara processors works on an annual cycle rather than a
    multi-year commitment to a single release.
    Each production SDK release is supported for one year. During that window, we provide defect fixes — no feature additions. For AM65
    specifically, we're now on one LTS refresh per year, so critical bug fixes between releases are available via our CI/CD snapshots.

    After the one-year window, bug fixes to TI components are made on the latest SDK version. Porting those fixes back to an older
    release would be on your side, though we're happy to support questions during that process as best as we can. Backports are typically not provided by
    us.

    On AM65, we have maintained our annual LTS release commitment since 2018 — that's 8 years of consistency. For general-purpose
    devices, sustained LTS releases are a commitment, and the retrospective release history reflects that. Each year's LTS release
    follows the same development and release cycle, providing continued coverage as long as the Linux community continues to support
    the underlying architecture, toolchains, and frameworks for that processor family.

    That said, AM65 is now in limited design support as noted on the product page, which is worth factoring into long-term planning.
    Each year we review overall customer engagement and forecast to determine whether continued software investment is warranted. So
    for new designs, where possible, we'd recommend considering newer devices like AM64x. We can also point you to third-party support
    providers if you need extended support for a design family that is in the limited design support category.

    Hope this helps. Let us know if you have more questions.

    A colleague will follow up on your CRA queries in the next few days.