Other Parts Discussed in Thread: SYSBIOS
Hi,
We tested execution time in cache invalidate and cache write back using the sysBIOS and also the CSL cache functions:
CACHE_invL1d(Vector, VectorLength, CACHE_WAIT)
Cache_inv(Vector, VectorLength, Cache_Type_L1D, CACHE_WAIT)
CACHE_wbL1d(Vector, VectorLength, CACHE_WAIT) ,
Cache_wb(Vector, VectorLength, Cache_Type_L1D, CACHE_WAIT)
1.- With sysbios functions, Cache_inv and Cache_wb with parameter CACHE_WAIT and CACHE_NOWAIT, the waiting time for both of them is very similar, seems that in the two cases (wait and no wait), the routine waits until the end of the transfer?
2.- For CACHE_invL1d and CACHE_wbL1d of CSL compared with Cache_wb and Cache_inv of the sysbios, for both of them with parameter WAIT for cache line transfer (64 bytes) we received:
Cache_inv =0.44 uSec
CACHE_invL1d =0.06 uSec
Cache_wb =0.43 uSec
CACHE_wbL1d =0.3 uSec
Waiting time for CSL routines is significantly shorter than sysbios routines times. Are the execution times right?
3.- We run our application under sysbios. Is possible to use the CSL routines aforementioned instead of the sysbios cache routines?
4.- In CSL CACHE_invL1d, the waiting time using the parameter CACHE_WAIT_FENCE is shorter than the same routine with parameter CACHE_WAIT. Does cover the use of CACHE_WAIT parameter, the case of CACHE_WAIT_FENCE parameter?
Thanks in advance.
Shmuel