This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Missing data in AM335x Datasheet (DDR3 Routing Specification)

Hello,

We need confirmation about the AM3359 datasheet's missing data and a typo.

No 1.
Regarding the DDR3 Routing Specification,
There is a missing data in the pg 170: "Table 5-59. CK and ADDR_CTRL Routing Specification".
The MAX value for "Rcp" (No.19) is not mentioned properly.

Can we assume the MAX value as Zo + 1?

No.2
Regarding the DDR3 Electrical Characteristics,
pg84 "Table 3-7. DC Electrical Characteristics" mentions VIL(Low-level input voltage)
MAX value as "VDDS_DDR - 0.1", is this a TYPO?
we believe that value would be "DDR_VREF - 0.1" instead.

Can we assume the VIL MAX value as DDR_VREF - 0.1?

Regards.
  • Thanks for bringing these data sheet issues to our attention.

    No 1.  Your assumption is correct.  I will submit this update to the next revision of the data sheet.

    No 2. You are correct VDDS_DDR - 0.1 should be DDR_VREF - 0.1.  You are the second person to highlight this issue and the update has already been submitted to the next revision of the data sheet.

    Regards,
    Paul