This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About DM8127 ARM frequency setting.

Genius 3400 points


Hi all,

        The current PLL settings of DM8127 is the following:

ARM clk: 600MHz
DDR clk: 400MHz
IVA clk: 450MHz
ISS clk: 400MHz
DSP clk: 400MHz
DSS clk: 200MHz 

I know the DM8127 in IPNC is 1GHz,  If I want to set ARM to 720MHz , 900MHz or 1GHz, how to set the  frequency of others(such as DDR, ISS, DSS etc.)?  what's the relation of them? which document I can get it?

Thanks a lot.