This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Using c64plus-imglib make

Hi.

I'm Sangyun.

I can't using English very well.

I study c64plus-imglib.

So I download c64plus-imglib.

And Setup this.

I want use Img lib, so read spruf30a(include c64plus-imglib) doc.

In doc 2.2 Using IMGLIB2 is exist.

Is imglib2.l64p necessary in order to work with dsp?
 
I want know  in detail 2.2.1.
 
"cl6x main.c -z -o IMG_boundary_drv.out -lrts64plus.lib -limglib2.l64P"
 
I have trouble with to add the sentence in upper line to which 'Makefile' located at and where to use 'make'.
 
I want know method.(link and make).

And where is rts64plus?

I can't serch.
 
Please answer for my answer in detail, plz.
 
Thank you.