Part Number: AM2732-Q1
Other Parts Discussed in Thread: SYSCONFIG
Dear TI Team,
I want to test about McASP function using am273x-evm.
- Imported the empty sample project for FreeRTOS.
- Set the SysConfig in each processor project's properties to the latest version.
- Added McASP TX/RX callback functions to the C66 project.
- Added McASP(A) to SysConfig in the C66 project, and configured the callback functions, serializers, and respective pins.
At this stage, the error shown in the following image is occurring.

How can this error be resolved?
Our environment is:
CCS : 21.0.1
SysConfig : 1.28.1
MCU+ SDK for AM273x : 12.0.0.29
Thanks, BR