Part Number: AM625
Other Parts Discussed in Thread: LM60430, TPS22965
Creating this thread to track feedback and updates on the updated schematic based on AM6254.
Schematics and files to be shared directly to Sreenivasa via email.
Hello Brian,
Thank you for the schematic review request.
Let me verify the provided inputs and come back.
Regards,
Sreenivasa
Hello Brian,
In case customer has a block diagram, review efficiency increases.
Is there a timeline Vertiv or you have in mind for me to check on the feasibility.
Regards,
Sreenivasa
Hello Brian,
I see your below message on email and please refer below inputs:
What would you like me to share with Gene and Vertiv in terms of your turnaround time for schematic reviews at this time?
In case the review is a priority holding their PCB release i will do my best to support by 21..23 November
Regards,
Sreenivasa
Hello Brian,
I did a quick check and have the below query that could affect the board power architecture.
Customer is using V_SDIO to power many of the attached devices including Ethernet Switch as against NVCC_3V3
V_SDIO LDO1 can be switched between 3.3V and 1.8V. Customer need to ensure the VSEL_SD is always pulled high and is not controlled.
With this configuration the SD card interface can support only legacy speed.
Please confirm with Customer if they would want UHS-I SD card support.
FYI, LM60430 is a 3.8-V to 36-V, 3-A, ultra-small synchronous step-down converter that is used to generate NVCC_3V3 and can support sourcing current for SOC IO and the attached peripherals IO supply.
Regards,
Sreenivasa
Hello Brian,
Page 12
RESETREQ_N connection not visible
Change net name to
RESET_N
R173
Reduce series resistor when connected to an SOC IO
SW_RESETz
Connect to one of the SOC IO

Reference

451340_REVA
Regards,
Sreenivasa
Hello Brian,
Please add your comments on the below for me to plan the review.
Hello Brian,
In case customer has a block diagram, review efficiency increases.
Is there a timeline Vertiv or you have in mind for me to check on the feasibility.
Regards,
Sreenivasa
Regards,
Sreenivasa
Hi Sreenivasa,
I am still waiting for a response from the customer - will reply when I know more.
Hello Brian,
Thank you.
I am assuming the inputs added above are also being shared.
Regards,
Sreenivasa
Hello Brian,
Can you please check if customer can share 420101G1 board information.
This improved review efficiency.
Customer did not add any shield between the signals.
The recommendation is to add ground shield between the processor IO signals.

Regards,
Sreenivasa
I will pass on your request and comment now. Appreciate the continued support.
From previous comments:
Customer is using V_SDIO to power many of the attached devices including Ethernet Switch as against NVCC_3V3
Customer: There is a power listing on the first page of the schematics, that is as close as I have gotten to a block diagram.
V_SDIO LDO1 can be switched between 3.3V and 1.8V. Customer need to ensure the VSEL_SD is always pulled high and is not controlled.
Customer: VSEL_SD should have been pull high - you are correct and that is reflected in current
With this configuration the SD card interface can support only legacy speed. Will you need UHS-I SD card support?
Customer: I would like to strive to make this the best possible design; what do I need to do for UHS-I SD card support?
FYI, LM60430 is a 3.8-V to 36-V, 3-A, ultra-small synchronous step-down converter that is used to generate NVCC_3V3 and can support sourcing current for SOC IO and the attached peripherals IO supply.
Customer: I am not certain what you are trying to tell me here, but I agree with what you have said.
Hello Brian,
Thank you for following up with customer:
FYI, LM60430 is a 3.8-V to 36-V, 3-A, ultra-small synchronous step-down converter that is used to generate NVCC_3V3 and can support sourcing current for SOC IO and the attached peripherals IO supply.
Customer: I am not certain what you are trying to tell me here, but I agree with what you have said.
U7 - V_3V3 - 3.3V MAIN
TI's LM60430 is a 3.8-V to 36-V, 3-A, ultra-small synchronous step-down converte
U8 - NVCC_3V3 3.3V SYS
TPS22965 5.7-V, 6-A, 16-mΩ On-Resistance Load Switch
V_SDIO can be replaced by NVCC_3V3 for all the attached devices.
V_SDIO can be used to source only VDDSHV5 and the SD card interface pullups to implement UHS-I SD card.
Additionally load switch and load switch reset logic as highlighted below needs to be implemented to support UHS-I SD card

Regards,
Sreenivasa
Hello Brian,
Customer is using V_SDIO to power many of the attached devices including Ethernet Switch as against NVCC_3V3
Customer: There is a power listing on the first page of the schematics, that is as close as I have gotten to a block diagram.
V_SDIO LDO1 can be switched between 3.3V and 1.8V. Customer need to ensure the VSEL_SD is always pulled high and is not controlled.
Customer: VSEL_SD should have been pull high - you are correct and that is reflected in current
The above reply answers these questions.
The SYS voltage is recommended to be used for SOC IO supply as well as attached device IO supply.
V_SDIO which is a switched 3.3V/1.8V IO can be used for VDDSHV5 + SD card interface pullups.
Regards,
Sreenivasa
Hello Brian,
Page 13 USB interface
USB0
Based on the configuration, i assume customer has USB0 configured as host.
VBUS divider is optional for Host.
In case customer wants to provision for VBUS divider (required for device, DFU boot configuration), the recommendation is to follow tithe USB VBUS design guidelines as per the data sheet. Please refer below reference diagram.
Add provision to bypass the CMC using 0R
P3
Not sure on the CC pin use case
Should a 5.1K be provisioned

Reference Schematic

USB1 Interface
Not sure on the USB interface configuration:
When USB1 is not used, leave the pin unconnected
When configured as host, VBUS is optional
When configured as device, a switched 5V through a divider that can be disconnected at the end of the session is recommended
Regards,
Sreenivasa
Hello Brian,
Checking if you heard from the customer regarding the expected timeline.
If this is a rush, given the number of changes i can support a quick sync call with customer to explain the changes to make if fast.
Regards,
Sreenivasa