This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

problem when flashing nand on DM8148 EVM board, using XDS100V2



The XDS100V2 emulator can't connect to the target.

following the "DM814x AM387x PSP Flashing Tools Guide"

       I changed the BTMODE[4:0]=00000

  • Connect the Spectrum Digital XDS560V2 STM USB emulator to the DM814x EVM
  • Start CCS by navigating to 'Start' menu in Windows XP
  • Select the workspace folder where you want to store your project
    • Select "View -> Target Configurations"
    • In the "Target Configurations" tab select "New Target Configuration File" button (in the top left corner)
    • Name the file (example, ti814x_usb.ccxml)
    • Click "Finish"
    • Connection = Spectrum Digital TI XDS560V2 STM USB Emulator(I changed to Texas Instrument XDS100V2 USB Emulator)
    • Board or Device = TI814x
    • Save configuration
    • From next run, the project and target configuration will be readily available and can be skipped
  • Select "Debug Perspective" in CCS if you are not there already: Window --> Open Perspective --> CCS Debug
  • Select View -> Target Configurations.
  • Expand "User Defined" configuration tree, Right click on the newly created target configuration and select "Launch Selected Configuration"
  • This should launch debug session
  • In Debug view, (scroll till the end) Select "Spectrum Digital XDS560V2 STM USB Emulator_0/Cortex A8" connection.
  • Right click on the Cortex A8 core listed and click on "Connect Target" , then the CCS does not responding any more.

My windows has recognize the XDS100V2 emulator yet.

My DM8148EVM is Mistral DDR3 PG2.1.

CCS version 4.3.4.00004.