Part Number: AM6442
Hi,
Could you let me know if AM6442 supports below clock output?
Clock is SI5332B-D-GM3.

Thanks.
Hello David,
The AM6442's general-purpose clock inputs (MCU_OSC0, MCU_EXT_REFCLK0, and EXT_REFCLK1) are specified as single-ended LVCMOS inputs (1.8V or 3.3V domains), not differential LVDS receivers. As configured, your SI5332B-D-GM3 output, per the table you provided, is programmed for LVDS signaling (V_SEPP ≈ 0.3–0.45 V_PP, V_CM ≈ 1.125–1.275V), which is not electrically compatible with the AM6442's LVCMOS input requirements.
Per the products datasheet, your SI5332B-D-GM3 is a blank, in-system programmable device- it is not factory-locked to LVDS. This means the output signal format is fully user-configurable via Skyworks' ClockBuilder Pro software over I²C, either at power-up or programmed into NVM for your production configuration.
Simply reconfigure the relevant output channel on the Si5332B from LVDS to LVCMOS (matching the 1.8V or 3.3V voltage domain of the AM6442 input you're driving) using ClockBuilder Pro.
Could you please confirm:
Best Regards,
Borislav Lazarkov
Hi Borislav,
Thanks for your support.
MCU_OSC0 is 1.8V
clock is from the master unit not customer's application.
For EXT_REFCLK0 and EXT_REFCLK1, it will support below red box specification.
Do you need detailed voltage?

Hello David,
To summarize the compatibility status for each input:
1. MCU_OSC0 (1.8V) — driven from master unit clock: From the AM6442 datasheet Table 6-24. MCU_OSC0 LVCMOS Digital Clock Source Requirements, MCU_OSC0_XI only accepts a single-ended 1.8V LVCMOS square-wave digital clock. It does not support a differential LVDS input. As configured in your table (LVDS, V_SEPP 0.3–0.45 V_PP, V_CM 1.125–1.275V), the Si5332 output is not directly compatible with MCU_OSC0. Reconfigure the relevant Si5332 output channel to 1.8V LVCMOS mode to drive MCU_OSC0_XI directly, since your SI5332B-D-GM3 is a blank, in-system programmable part and each output is independently configurable.
2. EXT_REFCLK0 and EXT_REFCLK1: Per the AM6442 pin attribute table, both EXT_REFCLK0 and EXT_REFCLK1 are also specified as single-ended LVCMOS inputs (buffer type: LVCMOS), supporting either 1.8V or 3.3V I/O voltage domains, not differential LVDS.
Since AM6442's EXT_REFCLK0/1 pins are LVCMOS-only (not LVDS-capable), the LVDS output spec you referenced (V_SEPP, V_CM, Table 5.7) would still need to be converted to single-ended LVCMOS before connecting to these pins, the same constraint as MCU_OSC0.
Do you need detailed voltage?
Yes, please share the detailed voltage/signal parameters you're planning for EXT_REFCLK0/1, specifically which voltage domain, 1.8V or 3.3V, and whether the Si5332 output on that path will also be configured to LVCMOS. That will let us confirm pin-level compatibility (VIH/VIL thresholds, duty cycle, rise/fall time) against the AM6442 clock timing requirements in Table 6-20.
Best Regards,
Borislav Lazarkov