This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Can AM3517EVM rotate video picture to 270degrees ?

Hi

    I have a question about AM3517EVM video display function.
   
    Can AM3517EVM rotate video picture to 270degrees ?
   
    Here are condition and environment.
   
    - Video signal is NTSC formatted and it is input to composite input
     terminal(J8).

    - Output(LCD display) size is SVGA (800x600).

    - Patch [dma-contig-to-free-pages.txt] is already applied.

    - Developed based on "ti-sdk-am3517-evm-05.02.00.00"  environment.

    - PSP is below  
        <x-loader>x-load-1.51-psp04.02.00.07  
        <uboot>u-boot-2010.06-psp04.02.00.07.sdk  
        <kernel>linux-2.6.37-psp04.02.00.07
    - Software is "userptr_loopback.c"

    Any informations and mentions are very helpful and appreciate.

Regards,
Nagasawa.