This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

6455,GPIO



hello,

I  use  the  GPIO7  for EDMA3.but  the  EDMA3  can't  work  although I  have  put  interrupt   in  the  GPIO7.

BUT  when  i   run   the  GPIO   example  of  the  CSL_6455  to  get  the  interrupt  of GPIO7,  it  can  detect  the   interrupt.  After  that  i   run  the  EDMA3 ,it  can  transfer  then.

I  don't   know  why?it  is  wether  that   i   need  to  open  the  GPIO7   before   i  use   it   for  the EDMA3?

Thank  you!I  need  your  help .

  • Hu Shushu,

    The interrupt is not required for EDMA to operate but the GPIO configuration is required. If you run the same GPIO initialization but do not link it to an interrupt, it would seem from your comments above that the GPIO would work - even without the interrupt occurring.

    Regards,
    RandyP

     

    If you need more help, please reply back. If this answers the question, please click  Verify Answer  , below.