This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

VFP



/QRfpe- Enable Hardware Floating-Point Targeting (Windows Embedded Compact 7)

This option (/QRfpe-) specifies that the compiler generate code that targets the vector floating-point (VFP) hardware on ARM family processors. If you are developing an application that targets an OS that utilizes VFP, you might need to specify that the OS must either be in RunFast mode or support instruction bouncing.

 How do I specify that the OS is set to RunFast mode or support instruction bouncing? How do I verify what state it is presently?

Thanks,