Hello,
I have a TMS320C5515 EVM Board (Rev B) with an ADS1x98ECG FE Board (Rev C). I am following the instructions in the following URL:
http://www.ti.com/general/docs/lit/getliterature.tsp?literatureNumber=sprabj1&fileType=pdf
I have been successful in downloading the compiled code to the EVM and running it. However, I see no wave signal on the LCD. I only see "ECG Monitor\n II o HR: BPM". I have tried with and without the ECG cable connected. I would assume that if there is no signal from the ADS1x98ECG FE Board, there would be a flat line? I have also tried with the electrodes of the ECG hooked up to another person, still nothing. Any ideas? I am new to working with these boards, so any insight would be greatly appreciated. Thanks.