This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Problem in 1080I capture using Capture-Encode demo



Hi ,

I am trying to capture 1080I using OMX capture-encode demo and display on LCD on DM8148 EVM .

I have followed the below TI Forum link for modifying the Capture-Encode Demo to support 1080I (interlaced ) capture ,i have made all the changes that are mentioned in the link .

http://e2e.ti.com/support/dsp/davinci_digital_media_processors/f/717/t/131887.aspx#475028

I am using a DVD player which is providing the Video input 1080I @ 25fps to the DM8148EVM .

The problem is that i am not getting a proper display on LCD ,i see two images ,one extended image getting overlapped with the other normal image .I have done

algEnable.bAlgBypass = 0 which should enable the DEI algorithm ,and i should  get a correct display .

I doubt whether DEI component is deinterlacing ,is there any other way to enable the DEI algorithm ? Is it the Color format issuse? DEI output buffers are in YUV422I format ,should i change it to YUV420SP?

when the application exits ,i get a below error message .

tearing down the capture-encode example
 exiting thread
 exiting thread
 exiting thread
 exiting thread
 got eventState changed to: OMX_StateIdle
 capture state idle
 got eventState changed to: OMX_StateIdle
 control tvp state idle
 got eventState changed to: OMX_StateIdle
 DEI state idle
 got eventState changed to: OMX_StateIdle
 display state idle
 got eventState changed to: OMX_StateIdle
 display control state idle
 got eventState changed to: OMX_StateIdle
 Encoder state idle
 got eventState changed to: OMX_StateLoaded
 display state loaded
 got eventState changed to: OMX_StateLoaded
 ctrl-dc state loaded
 got eventState changed to: OMX_StateLoaded
 encoder state loaded
 got event*** unrecoverable error: OMX_ErrorUndefined (0x80001001)
Press a key to proceed

./loggerSMDump.out 0x9E400000 0x100000 all

N:VPSS  P:2 #:01303 T:000000136612dc05 S:Entered Function :omxrpc_skel_freebuffer
N:VPSS  P:2 #:01304 T:0000001366162023 S:drivers/m2m/src/vpsdrv_m2mDei.c @ Line 522:
N:VPSS  P:2 #:01305 T:000000136616b863 S:Context fields are not retrived back. Try FVID2_stop ()                  before closing!!
N:VPSS  P:2 #:01307 T:000000136618a989 S:Entered Function :omxrpc_skel_freebuffer
N:VPSS  P:2 #:01306 T:0000001366171a81 S: OMX Error in _OMX_VFPCDeiDualOutDelete :: line 1197
N:VPSS  P:2 #:01308 T:00000013661b9bb1 S: OMX Error in OMX_TI_VFPC_CommandNotify :: line 1303
N:VPSS  P:2 #:01309 T:00000013661be94b S: OMX Error in _OMX_BASE_HandleStateTransition :: line 371
N:VPSS  P:2 #:01310 T:00000013661c45d5 S:Module<OMX.TI.VPSSM3.VFPC.DEIMDUALOUT> Leaving<_OMX_BASE_HandleStateTransition> @line<482> with error<-2147479551:ErrorUndefined>
N:VPSS  P:2 #:01311 T:00000013661e2ba5 S:Entered Function :omxrpc_skel_freebuffer
N:VPSS  P:2 #:01312 T:0000001366225ffb S:Entered Function :omxrpc_skel_freebuffer
N:VPSS  P:2 #:01314 T:0000001366273c61 S:Entered Function :omxrpc_skel_freebuffer
N:VPSS  P:2 #:01313 T:000000136625fa83 S:Module<OMX.TI.VPSSM3.VFPC.DEIMDUALOUT> Leaving<OMX_BASE_PROCESS_CmdEvent> @line<784> with error<-2147479551:ErrorUndefined>
N:VPSS  P:2 #:01315 T:0000001366296917 S:Module<OMX.TI.VPSSM3.VFPC.DEIMDUALOUT> Leaving<OMX_BASE_CmdEventHandler> @line<466> with error<-2147479551:ErrorUndefined>
N:VPSS  P:2 #:01317 T:00000013662aaedd S:Entered Function :omxrpc_skel_freebuffer
N:VPSS  P:2 #:01316 T:000000136629e28b S:Module<OMX.TI.VPSSM3.VFPC.DEIMDUALOUT> Entering<OMX_BASE_CmdEventHandler> @line<434>

Can anyone help me where am i going wrong ?any help is appreciated .

Thanks,

N Sivaramkrishna.