Hi,
I am trying to run .moduletest.out drv_capture.The log is given below:
# ./moduletest.out drv_capture
DavinciDisplay DavinciDisplay.1: Before finishing with S_FMT:
layer.pix_fmt.bytesperline = 640,
layer.pix_fmt.width = 640,
layer.pix_fmt.height = 480,
layer.pix_fmt.sizeimage =460800
CLK Hz,
ARMDavinciDisplay DavinciDisplay.1: pixfmt->width = 640,
layer->layer_info.config.line_length= 640
Hz = 432000000
DDR Hz = 340000000
VPSS Hz = 3400000DavinciDisplay DavinciDisplay.1: Invalid crop values
00
IMCOP Hz = DavinciDisplay DavinciDisplay.1: Error in S_CROP params
340000000
DavinciDisplay DavinciDisplay.1: Invalid crop values
DRV LDC: GetConfDavinciDisplay DavinciDisplay.1: Error in S_CROP params
ig 0003 0x0
[ODavinciDisplay DavinciDisplay.1: Invalid crop values
SA_FILE ] ReadinDavinciDisplay DavinciDisplay.1: Error in S_CROP params
g file [/mnt/nand/IMG_Paramset.bin] ... ERROR
IMAGE TUNE: Paramset File is not available..... Setting DEFAULT parameter
CAPTURE: Opening display.
ERROR (drv_display.c|DRV_displaySetWinPos|679): VIDIOC_S_CROP ioctl
ERROR (drv_display.c|DRV_displaySetWinSize|701): VIDIOC_S_CROP ioctl
ERROR (drv_display.c|DRV_displayExpand|598): VIDIOC_S_CROP ioctl
CAPTURE: Opening capture on imager IMX036_3MP.
############OPEN###########
==========>>>> Start X,Y = 52,18
Sensor Mode Info,
Width = 1384
Height = 772
fps = 30
Bin Enable = 0
Sensor Frame Timing Info,
fps = 30
t_frame (ns) = 33333334.000000
t_row (ns) = 35687.500000
t_pclk (ns) = 15.625000
W = 1384
H = 772
SW = 1125
SD = 0
HB = 450
VB = 162
HBmin = 450
VBmin = 9
f_pclk = 64000000
shutterOverhead (ns) = 6656.250000
col_size = 1384
row_size = 772
col_bin = 0
row_bin = 0
col_start = 408
row_start = 524
pll_M = 16
pll_N = 1
pll_DIV = 1
############reset###########
############SPI OPEN###########
spi mode: 16
bits per word: 8
max speed: 12000000 Hz (12000 KHz)
############SET REG###########
############OPEN END###########
================> 512, 0, 1735
TI Setting Applied
After that there is no output.It hangs here.
This is coming from DRV_H3Aopen
and i think it is defined in some system file called system.ini and i
am not able to open this file.
how we can open system.ini file.
Thanks and Regards,
Mayank