Other Parts Discussed in Thread: AM3517
I have some problem in AM3517 OTG usb driver.
I configure it as device type in hardware and initialize it in software with:
UINIT = 0; <-- PDR interrupt
musbr->power = 0x60 <-- power musb
.// Enable all interrupt in core level and wrap levle
musbr->intrusbe = 0xff ;
musbr->intrrxe = 0xffff;
musbr->intrtxe = 0xffff;
...
// Open softe connect.
..
After initialize. i open OTG interrupt INT_71. Then OTG generate a suspend interrupt.
But when i connect USB to PC (host). Register "USB Endpoint Interrupt Source Register" = 0x01
It means a tx interrupt have generated. But can't trigger a INT_71 interrupt.
Why?
In int_71 service routine. i written 1 to CONTROL_LVL_INTR_CLEAR.D4 for interrupt clear.
Any one can help me?
Thanks.