This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

StarterWare with CriticalLink MityDSP-L138F



I have just purchased the MityDSP-L138F development board from CriticalLink.  My desire is to program it with StarterWare.  The board is different than the evmOMAP-L138 board.  The COM port is wired to UART1 instead of UART2 for one.  The beauty of StarterWare is that it can reduce my development time by providing high level code for the components, but if I have to understand all the intricacies of the board differences that is going to be costly in time.  I like the MityDSP board because it has an FPGA.

My question is, does anyone have a StarterWare build that uses the specifics of the MityDSP board instead of the evmOMAP board?  I can find info on TI's website of CriticalLink being a partner, but no info on support in StarterWare.

Thanks,

Tim