This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

sys_bootx pins on AM37x safe to directly connect

Is it safe to directly tie the sys_bootx pins on the AM37xx to logic high (1.8V) or GND without a pullup/pulldown resistor? I woudn't normally do this but space is at a premium and the boot configuration is now fixed and will not change.

The only thing I can think of that would be a problem is if the pin mux were set up wrong, but are there any other concerns?

Thanks,