Does the u-boot code, detect Netra Si version (PG1.1/2.0) and do DDR3 hardware or software leveling accordingly?
This question is due to Errata: Advisory 2.0.20 DDR3 Hardware Leveling Does Not Function Reliably
In revision 1.1, DDR3 hardware leveling does not function reliably, can be used with software leveling.
In 2.0 this is fixed and Hardware leveling can be used.