1. I already have a project with NDK+ c6747_audio_edma.prj and using this, I can receive voice from LineIn and transmit this voice out to another PC via UDP protocol (via ethernet cable). Now, I hear tic sound in the background and I doubt that there might be some other task preempting from sending out at the correct timing. To see what is happening with the task, I need the Exec graph- but I have dsp/bios ver5 installed. Do I need to install sys/bios ver 6 to use Exec graph?
2. Apart from this, do you think I should stick with dsp/bios 5 or should I migrate to sys/bios 6 for this voip application?
3. Could you pls send some examples using NDK + sys/bios 6 and also another example having c6747_audio_edma.prj (which is one of the example projects from TI) using sys/bios6?
ndk: 2.0
ccs ver 4.2.4.00033
edma3_lld_01_11_03_01
pspdrivers_01_30_01
bios_6_33_01_25 or any bios6 you suggest
xdctools_3_22_01_21