This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Which is shared region in default dsplink?

Hi,

   I am using "dvsdk_omapl138-evm_4_02_00_06" in ubuntu 10.04. When I see TCF file of dsplink sample applications. There are 2 region DSPLINKMEM and POOLMEM. What is Sections stands for and which is shared region?

                Where POOL_Config allocated memory?  For example consider MSGQ example, Where DSP QUEUE and GPP QUEUE is create (DSPLINKMEM or POOL MEM) ?

If My message contains only MSGQ_Header than what is size of my message?

How many number of msg can i able to allocate in a Queue?

What will be size of a Queue structure in shared region (if Queue has only one message holding capacity )?
 Will Size of Queue changes for GPP and DSP  side Queue?

I had gone through LNK_082_des  and LNK_031_des but i'ma not able to figure out this.

Please Help me...